EtherCAT Slave1.11.00

◆ EC_API_SLV_CiA402_registerLocalError()

void EC_API_SLV_CiA402_registerLocalError ( EC_API_SLV_SHandle_t pEcSlaveApi_p,
void *  pContext_p,
EC_API_SLV_CiA402_CBUsrApplLocalError_t  cbFunc_p 
)

Register a local error function, triggered if CiA402 state machine changes into an error state.

Parameters
[in]pEcSlaveApi_pEtherCAT DTK instance.
[in]pContext_pCallback context
[in]cbFunc_pCiA402 Application.
Example
#include <ecSlvApi.h>
// required variables
EC_API_SLV_CiA402LocalError cbFunc;
// the Call
retVal = EC_API_SLV_CiA402_registerLocalError(ecSlaveApi, cbFunc);
See also
EC_API_SLV_CiA402_registerStateMachine
Examples
ecSlvESI.c.
EC_API_SLV_SHandle_t
struct EC_API_SLV_SHandle EC_API_SLV_SHandle_t
EC_API_SLV_SHandle_t describes the EtherCAT Slave API.
Definition: ecSlvApi.h:149
EC_API_SLV_CiA402_registerLocalError
void EC_API_SLV_CiA402_registerLocalError(EC_API_SLV_SHandle_t *pEcSlaveApi_p, void *pContext_p, EC_API_SLV_CiA402_CBUsrApplLocalError_t cbFunc_p)
Register a local error function, triggered if CiA402 state machine changes into an error state.
Definition: ecSlvApi_CiA402Stub.c:267