AM243x MCU+ SDK  08.05.00
DDR_EccRegion Struct Reference

Detailed Description

DDR Inline ECC region The structure specifies the DDR inline ECC region start and End address.

Data Fields

uint32_t ddrEccStart0
 
uint32_t ddrEccEnd0
 
uint32_t ddrEccStart1
 
uint32_t ddrEccEnd1
 
uint32_t ddrEccStart2
 
uint32_t ddrEccEnd2
 

Field Documentation

◆ ddrEccStart0

uint32_t DDR_EccRegion::ddrEccStart0

DDR inline ECC region-0 start address

◆ ddrEccEnd0

uint32_t DDR_EccRegion::ddrEccEnd0

DDR inline ECC region-0 end address

◆ ddrEccStart1

uint32_t DDR_EccRegion::ddrEccStart1

DDR inline ECC region-1 start address

◆ ddrEccEnd1

uint32_t DDR_EccRegion::ddrEccEnd1

DDR inline ECC region-1 end address

◆ ddrEccStart2

uint32_t DDR_EccRegion::ddrEccStart2

DDR inline ECC region-2 start address

◆ ddrEccEnd2

uint32_t DDR_EccRegion::ddrEccEnd2

DDR inline ECC region-2 end address