AM243x MCU+ SDK  08.05.00

Detailed Description

Broadcast/multicast bandwidth limit configuration parameters.

Data Fields

uint32_t portNum
 
bool bcastRateLimitForPortEn
 
bool mcastRateLimitForPortEn
 
uint32_t bcastLimitNumPktsPerSec
 
uint32_t mcastLimitNumPktsPerSec
 

Field Documentation

◆ portNum

uint32_t CpswAle_PortBcastMcastRateLimitParams::portNum

Port number for which broadcast/multicast rate limiting configuration is to be done

◆ bcastRateLimitForPortEn

bool CpswAle_PortBcastMcastRateLimitParams::bcastRateLimitForPortEn

Enable Broadcast Rate Limit for port. If set to TRUE, bcastLimitNumPktsPerSec should be non-zero

◆ mcastRateLimitForPortEn

bool CpswAle_PortBcastMcastRateLimitParams::mcastRateLimitForPortEn

Enable Multicast Rate Limit for port. If set to TRUE, mcastLimitNumPktsPerSec should be non-zero

◆ bcastLimitNumPktsPerSec

uint32_t CpswAle_PortBcastMcastRateLimitParams::bcastLimitNumPktsPerSec

Broadcast packet limit per second

◆ mcastLimitNumPktsPerSec

uint32_t CpswAle_PortBcastMcastRateLimitParams::mcastLimitNumPktsPerSec

Multicast packet limit per second