AM243x MCU+ SDK  08.05.00

Introduction

This module contains APIs to program and use DMA drivers available in the SoC with UART.

Data Structures

struct  UART_DmaFxns
 Driver implementation callbacks. More...
 
struct  UART_DmaConfig
 UART DMA Configuration, these are filled by SysCfg based on the DMA driver that is selected. More...
 

Functions

UART_DmaHandle UART_dmaOpen (UART_Handle uartHandle, int32_t index)
 API to open an UART DMA channel. More...
 
int32_t UART_dmaClose (UART_Handle handle)
 API to close an UART DMA channel. More...
 
int32_t UART_dmaDisableChannel (UART_Handle handle, uint32_t isChannelTx)
 API to disable an DMA channel. More...
 
int32_t UART_writeInterruptDma (UART_Object *obj, const UART_Attrs *attrs, UART_Transaction *transaction)
 API to write data using an UART DMA channel. More...
 
int32_t UART_readInterruptDma (UART_Object *obj, const UART_Attrs *attrs, UART_Transaction *transaction)
 API to read data using an UART DMA channel. More...
 

Typedefs

typedef void * UART_DmaHandle
 Handle to the UART DMA Config Object returned by UART_dmaOpen. More...
 
typedef int32_t(* UART_dmaOpenFxn) (UART_Handle uartHandle, void *uartDmaArgs)
 Driver implementation to open a specific DMA driver channel - UDMA, EDMA etc. More...
 
typedef int32_t(* UART_dmaTransferReadFxn) (UART_Object *obj, const UART_Attrs *attrs, UART_Transaction *transaction)
 Driver implementation to do a DMA read using a specific DMA driver - UDMA, EDMA etc. More...
 
typedef int32_t(* UART_dmaTransferWriteFxn) (UART_Object *obj, const UART_Attrs *attrs, UART_Transaction *transaction)
 Driver implementation to do a DMA write using a specific DMA driver - UDMA, EDMA etc. More...
 
typedef int32_t(* UART_dmaCloseFxn) (UART_Handle handle)
 Driver implementation to close a specific DMA driver channel - UDMA, EDMA etc. More...
 
typedef int32_t(* UART_dmaDisableChannelFxn) (UART_Handle handle, uint32_t isChannelTx)
 Driver implementation to diisable a specific DMA driver channel - UDMA, EDMA etc. More...
 

Typedef Documentation

◆ UART_DmaHandle

typedef void* UART_DmaHandle

Handle to the UART DMA Config Object returned by UART_dmaOpen.

◆ UART_dmaOpenFxn

typedef int32_t(* UART_dmaOpenFxn) (UART_Handle uartHandle, void *uartDmaArgs)

Driver implementation to open a specific DMA driver channel - UDMA, EDMA etc.

Typically this callback is hidden from the end application and is implemented when a new DMA driver needs to be supported.

Parameters
uartHandle[in] UART Handle
uartDmaArgs[in] DMA specific arguments, obtained from the config
Returns
SystemP_SUCCESS on success, else failure

◆ UART_dmaTransferReadFxn

typedef int32_t(* UART_dmaTransferReadFxn) (UART_Object *obj, const UART_Attrs *attrs, UART_Transaction *transaction)

Driver implementation to do a DMA read using a specific DMA driver - UDMA, EDMA etc.

Typically this callback is hidden from the end application and is implemented when a new DMA driver needs to be supported.

Parameters
obj[in] Pointer to UART object
attrs[in] Pointer to UART attributes.
transaction[in] Pointer to UART_Transaction. This parameter can't be NULL
Returns
SystemP_SUCCESS on success, else failure

◆ UART_dmaTransferWriteFxn

typedef int32_t(* UART_dmaTransferWriteFxn) (UART_Object *obj, const UART_Attrs *attrs, UART_Transaction *transaction)

Driver implementation to do a DMA write using a specific DMA driver - UDMA, EDMA etc.

Typically this callback is hidden from the end application and is implemented when a new DMA driver needs to be supported.

Parameters
obj[in] Pointer to UART object.
attrs[in] Pointer to UART attributes.
transaction[in] Pointer to UART_Transaction. This parameter can't be NULL
Returns
SystemP_SUCCESS on success, else failure

◆ UART_dmaCloseFxn

typedef int32_t(* UART_dmaCloseFxn) (UART_Handle handle)

Driver implementation to close a specific DMA driver channel - UDMA, EDMA etc.

Typically this callback is hidden from the end application and is implemented when a new DMA driver needs to be supported.

Parameters
handle[in] UART handle returned from UART_open
Returns
SystemP_SUCCESS on success, else failure

◆ UART_dmaDisableChannelFxn

typedef int32_t(* UART_dmaDisableChannelFxn) (UART_Handle handle, uint32_t isChannelTx)

Driver implementation to diisable a specific DMA driver channel - UDMA, EDMA etc.

Parameters
handle[in] UART handle returned from UART_open
isChannelTx[in] Variable to indicate if it is TX/RX Channel
Returns
SystemP_SUCCESS on success, else failure

Function Documentation

◆ UART_dmaOpen()

UART_DmaHandle UART_dmaOpen ( UART_Handle  uartHandle,
int32_t  index 
)

API to open an UART DMA channel.

This API will open a DMA Channel using the appropriate DMA driver callbacks and the registered via Sysconfig

Parameters
uartHandle[in] UART Handle
index[in] Index of the DMA Config selected for this particular UART driver instance
Returns
Handle to the UART DMA Config Object

◆ UART_dmaClose()

int32_t UART_dmaClose ( UART_Handle  handle)

API to close an UART DMA channel.

Parameters
handle[in] UART handle returned from UART_open
Returns
SystemP_SUCCESS on success, else failure

◆ UART_dmaDisableChannel()

int32_t UART_dmaDisableChannel ( UART_Handle  handle,
uint32_t  isChannelTx 
)

API to disable an DMA channel.

Parameters
handle[in] UART handle returned from UART_open
isChannelTx[in] Variable to indicate if it is TX/RX Channel
Returns
SystemP_SUCCESS on success, else failure

◆ UART_writeInterruptDma()

int32_t UART_writeInterruptDma ( UART_Object obj,
const UART_Attrs attrs,
UART_Transaction transaction 
)

API to write data using an UART DMA channel.

Parameters
obj[in] Pointer to UART object
attrs[in] Pointer to UART attributes
transaction[in] Pointer to UART_Transaction. This parameter can't be NULL
Returns
SystemP_SUCCESS on success, else failure

◆ UART_readInterruptDma()

int32_t UART_readInterruptDma ( UART_Object obj,
const UART_Attrs attrs,
UART_Transaction transaction 
)

API to read data using an UART DMA channel.

Parameters
obj[in] Pointer to UART object
attrs[in] Pointer to UART attributes
transaction[in] Pointer to UART_Transaction. This parameter can't be NULL
Returns
SystemP_SUCCESS on success, else failure