AM243x MCU+ SDK  08.05.00

Introduction

This module contains APIs to program and use the SA2UL.

Files

file  sa2ul.h
 This file contains the prototype of SA2UL driver APIs.
 

Data Structures

struct  SA2UL_ContextParams
 Parameters passed to SA2UL_contextAlloc() More...
 
struct  SA2UL_Params
 Parameters passed to SA2UL_open() More...
 
struct  SA2UL_Object
 Object for a SA2UL crypto operation. More...
 
struct  SA2UL_Attrs
 SA2UL instance attributes - used during init time. More...
 
struct  SA2UL_Config
 SA2UL driver context. More...
 
struct  SA2UL_MCEData
 MEDdata for Encryption engine. More...
 
struct  SA2UL_SecCtxAuth
 SA2UL context RAM structure for authentication engine. More...
 
struct  SA2UL_Scctl
 SA2UL SC control structure. More...
 
struct  SA2UL_SecCtxEnc
 SA2UL context RAM structure for Encryption engine. More...
 
struct  SA2UL_SecCtx
 SA2UL context RAM structure. More...
 
struct  SA2UL_ContextObject
 SA2UL context object structure. More...
 

Functions

void SA2UL_init (void)
 This function initializes the SA2UL module. More...
 
void SA2UL_deinit (void)
 This function de-initializes the SA2UL module. More...
 
SA2UL_Handle SA2UL_open (uint32_t index, const SA2UL_Params *params)
 This function opens a given SA2UL module. More...
 
void SA2UL_close (SA2UL_Handle handle)
 Function to close a SA2UL module specified by the SA2UL handle. More...
 
int32_t SA2UL_contextAlloc (SA2UL_Handle handle, SA2UL_ContextObject *ctxObj, const SA2UL_ContextParams *ctxPrms)
 Function to configure secure context. More...
 
int32_t SA2UL_contextFree (SA2UL_ContextObject *pCtxObj)
 Function to free secure context configuration. More...
 
int32_t SA2UL_contextProcess (SA2UL_ContextObject *ctxObj, const uint8_t *input, uint32_t ilen, uint8_t *output)
 Function to transfer and recieve data buffer. More...
 
static void SA2UL_Params_init (SA2UL_Params *prms)
 Function to initialize default SA2UL parameters. More...
 
int32_t SA2UL_rngSetup (SA2UL_Handle handle)
 setup the SA2UL RNG module. More...
 
int32_t SA2UL_rngRead (SA2UL_Handle handle, uint32_t *out)
 Read random numbers into the output buffer. More...
 
static void SA2UL_ContextParams_init (SA2UL_ContextParams *ctxPrms)
 

Typedefs

typedef void * SA2UL_Handle
 Handle to the SA2UL driver returned by SA2UL_open() More...
 

Macros

#define SA2UL_ENC_KEYSIZE_BITS(k)   (128u + (64u * (k)))
 

SA2UL macros

#define SA2UL_MAX_HASH_SIZE_BYTES   (64U)
 Max hash size in bytes. More...
 
#define SA2UL_MAX_KEY_SIZE_BYTES   (32U)
 Max key size in bytes. More...
 
#define SA2UL_MAX_IV_SIZE_BYTES   (16U)
 Max Initialization vector (IV) size in bytes. More...
 
#define SA2UL_NUMBER_OF_RINGS   (3U)
 Max number of rings. More...
 
#define SA2UL_CACHELINE_ALIGNMENT   (16U)
 Cache line size for alignment of descriptor and buffers. More...
 
#define SA2UL_SECCTX_SIZE   (256U)
 Secure context memsize. More...
 
#define SA2UL_INSTANCES_MAX   (4U)
 Max SA2UL instances. More...
 
#define SA2UL_RING_N_ELEMS   (8U)
 Max SA2UL ring n elements. More...
 
#define SA2UL_SW_RING_NUM   (304U)
 Max SA2UL sw ring number. More...
 
#define SA2UL_MAX_INPUT_LENGTH_ENC   (0xFFFFU)
 Max Aes input length for encryption and decryption (64KB-1) More...
 
#define SA2UL_MAX_INPUT_LENGTH_AUTH   (0x3FFFFFU)
 Max input length for authentication (4MB-1) More...
 

SA2UL Algo Types

#define SA2UL_HASH_ALG_NULL   (0x10U)
 Hash Algo NULL. More...
 
#define SA2UL_HASH_ALG_SHA1   (0x12U)
 Hash Algo SHA-1. More...
 
#define SA2UL_HASH_ALG_SHA2_256   (0x14U)
 Hash Algo SHA-256. More...
 
#define SA2UL_HASH_ALG_SHA2_512   (0x16U)
 Hash Algo SHA-512. More...
 

SA2UL Operations Sequence

#define SA2UL_OP_ENC   (0x01U)
 SA2UL operations encryption. More...
 
#define SA2UL_OP_AUTH   (0x02U)
 SA2UL operations authentication. More...
 
#define SA2UL_OP_ENC_THEN_AUTH   (0x03U)
 SA2UL operation encryption then authentication. More...
 
#define SA2UL_OP_AUTH_THEN_ENC   (0x04U)
 SA2UL operations authentication then encryption. More...
 

SA2UL engine operation type

#define SA2UL_ENGINE_CODE_DEFAULT_ENGINE_ID   (0U)
 SA2UL default engine Id. More...
 
#define SA2UL_ENGINE_CODE_ENCRYPTION_MODULE_P1   (2U)
 SA2UL Encryption engine module p1. More...
 
#define SA2UL_ENGINE_CODE_ENCRYPTION_MODULE_P2   (3U)
 SA2UL Encryption engine module p2. More...
 
#define SA2UL_ENGINE_CODE_AUTHENTICATION_MODULE_P1   (4U)
 SA2UL Authentication engine module p1. More...
 
#define SA2UL_ENGINE_CODE_AUTHENTICATION_MODULE_P2   (5U)
 SA2UL Authentication engine module p2. More...
 
#define SA2UL_ENGINE_CODE_DEFAULT_EGRESS_PORT   (20U)
 SA2UL Default Engress Port. More...
 

SA2UL Encryption Algos

#define SA2UL_ENC_ALG_AES   (0x0U)
 SA2UL AES Encryption Algorithm. More...
 
#define SA2UL_ENC_ALG_TDES   (0x1U)
 SA2UL TDES Encryption Algorithm. More...
 
#define SA2UL_ENC_ALG_MAX   (0x2U)
 SA2UL Encryption Maximun number of Algorithms. More...
 

SA2UL Encryption direction

#define SA2UL_ENC_DIR_ENCRYPT   (0x0U)
 Encryption direction. More...
 
#define SA2UL_ENC_DIR_DECRYPT   (0x1U)
 Decryption direction. More...
 

SA2UL Encryption modes

#define SA2UL_ENC_MODE_ECB   (0x0U)
 ECB mode. More...
 
#define SA2UL_ENC_MODE_CBC   (0x1U)
 CBC mode. More...
 
#define SA2UL_ENC_MODE_MAX   (0x2U)
 Maximun Encryption modes. More...
 

SA2UL Encryption key sizes

#define SA2UL_ENC_KEYSIZE_128   (0x0U)
 Encryption 128 bit key size. More...
 
#define SA2UL_ENC_KEYSIZE_192   (0x1U)
 Encryption 192 bit key size. More...
 
#define SA2UL_ENC_KEYSIZE_256   (0x2U)
 Encryption 256 bit key size. More...
 
#define SA2UL_ENC_KEYSIZE_MAX   (0x3U)
 Max key size. More...
 

Macro Definition Documentation

◆ SA2UL_MAX_HASH_SIZE_BYTES

#define SA2UL_MAX_HASH_SIZE_BYTES   (64U)

Max hash size in bytes.

◆ SA2UL_MAX_KEY_SIZE_BYTES

#define SA2UL_MAX_KEY_SIZE_BYTES   (32U)

Max key size in bytes.

◆ SA2UL_MAX_IV_SIZE_BYTES

#define SA2UL_MAX_IV_SIZE_BYTES   (16U)

Max Initialization vector (IV) size in bytes.

◆ SA2UL_NUMBER_OF_RINGS

#define SA2UL_NUMBER_OF_RINGS   (3U)

Max number of rings.

◆ SA2UL_CACHELINE_ALIGNMENT

#define SA2UL_CACHELINE_ALIGNMENT   (16U)

Cache line size for alignment of descriptor and buffers.

◆ SA2UL_SECCTX_SIZE

#define SA2UL_SECCTX_SIZE   (256U)

Secure context memsize.

◆ SA2UL_INSTANCES_MAX

#define SA2UL_INSTANCES_MAX   (4U)

Max SA2UL instances.

◆ SA2UL_RING_N_ELEMS

#define SA2UL_RING_N_ELEMS   (8U)

Max SA2UL ring n elements.

◆ SA2UL_SW_RING_NUM

#define SA2UL_SW_RING_NUM   (304U)

Max SA2UL sw ring number.

◆ SA2UL_MAX_INPUT_LENGTH_ENC

#define SA2UL_MAX_INPUT_LENGTH_ENC   (0xFFFFU)

Max Aes input length for encryption and decryption (64KB-1)

◆ SA2UL_MAX_INPUT_LENGTH_AUTH

#define SA2UL_MAX_INPUT_LENGTH_AUTH   (0x3FFFFFU)

Max input length for authentication (4MB-1)

◆ SA2UL_HASH_ALG_NULL

#define SA2UL_HASH_ALG_NULL   (0x10U)

Hash Algo NULL.

◆ SA2UL_HASH_ALG_SHA1

#define SA2UL_HASH_ALG_SHA1   (0x12U)

Hash Algo SHA-1.

◆ SA2UL_HASH_ALG_SHA2_256

#define SA2UL_HASH_ALG_SHA2_256   (0x14U)

Hash Algo SHA-256.

◆ SA2UL_HASH_ALG_SHA2_512

#define SA2UL_HASH_ALG_SHA2_512   (0x16U)

Hash Algo SHA-512.

◆ SA2UL_OP_ENC

#define SA2UL_OP_ENC   (0x01U)

SA2UL operations encryption.

◆ SA2UL_OP_AUTH

#define SA2UL_OP_AUTH   (0x02U)

SA2UL operations authentication.

◆ SA2UL_OP_ENC_THEN_AUTH

#define SA2UL_OP_ENC_THEN_AUTH   (0x03U)

SA2UL operation encryption then authentication.

◆ SA2UL_OP_AUTH_THEN_ENC

#define SA2UL_OP_AUTH_THEN_ENC   (0x04U)

SA2UL operations authentication then encryption.

◆ SA2UL_ENGINE_CODE_DEFAULT_ENGINE_ID

#define SA2UL_ENGINE_CODE_DEFAULT_ENGINE_ID   (0U)

SA2UL default engine Id.

◆ SA2UL_ENGINE_CODE_ENCRYPTION_MODULE_P1

#define SA2UL_ENGINE_CODE_ENCRYPTION_MODULE_P1   (2U)

SA2UL Encryption engine module p1.

◆ SA2UL_ENGINE_CODE_ENCRYPTION_MODULE_P2

#define SA2UL_ENGINE_CODE_ENCRYPTION_MODULE_P2   (3U)

SA2UL Encryption engine module p2.

◆ SA2UL_ENGINE_CODE_AUTHENTICATION_MODULE_P1

#define SA2UL_ENGINE_CODE_AUTHENTICATION_MODULE_P1   (4U)

SA2UL Authentication engine module p1.

◆ SA2UL_ENGINE_CODE_AUTHENTICATION_MODULE_P2

#define SA2UL_ENGINE_CODE_AUTHENTICATION_MODULE_P2   (5U)

SA2UL Authentication engine module p2.

◆ SA2UL_ENGINE_CODE_DEFAULT_EGRESS_PORT

#define SA2UL_ENGINE_CODE_DEFAULT_EGRESS_PORT   (20U)

SA2UL Default Engress Port.

◆ SA2UL_ENC_ALG_AES

#define SA2UL_ENC_ALG_AES   (0x0U)

SA2UL AES Encryption Algorithm.

◆ SA2UL_ENC_ALG_TDES

#define SA2UL_ENC_ALG_TDES   (0x1U)

SA2UL TDES Encryption Algorithm.

◆ SA2UL_ENC_ALG_MAX

#define SA2UL_ENC_ALG_MAX   (0x2U)

SA2UL Encryption Maximun number of Algorithms.

◆ SA2UL_ENC_DIR_ENCRYPT

#define SA2UL_ENC_DIR_ENCRYPT   (0x0U)

Encryption direction.

◆ SA2UL_ENC_DIR_DECRYPT

#define SA2UL_ENC_DIR_DECRYPT   (0x1U)

Decryption direction.

◆ SA2UL_ENC_MODE_ECB

#define SA2UL_ENC_MODE_ECB   (0x0U)

ECB mode.

◆ SA2UL_ENC_MODE_CBC

#define SA2UL_ENC_MODE_CBC   (0x1U)

CBC mode.

◆ SA2UL_ENC_MODE_MAX

#define SA2UL_ENC_MODE_MAX   (0x2U)

Maximun Encryption modes.

◆ SA2UL_ENC_KEYSIZE_128

#define SA2UL_ENC_KEYSIZE_128   (0x0U)

Encryption 128 bit key size.

◆ SA2UL_ENC_KEYSIZE_192

#define SA2UL_ENC_KEYSIZE_192   (0x1U)

Encryption 192 bit key size.

◆ SA2UL_ENC_KEYSIZE_256

#define SA2UL_ENC_KEYSIZE_256   (0x2U)

Encryption 256 bit key size.

◆ SA2UL_ENC_KEYSIZE_MAX

#define SA2UL_ENC_KEYSIZE_MAX   (0x3U)

Max key size.

◆ SA2UL_ENC_KEYSIZE_BITS

#define SA2UL_ENC_KEYSIZE_BITS (   k)    (128u + (64u * (k)))

Typedef Documentation

◆ SA2UL_Handle

typedef void* SA2UL_Handle

Handle to the SA2UL driver returned by SA2UL_open()

Function Documentation

◆ SA2UL_init()

void SA2UL_init ( void  )

This function initializes the SA2UL module.

◆ SA2UL_deinit()

void SA2UL_deinit ( void  )

This function de-initializes the SA2UL module.

◆ SA2UL_open()

SA2UL_Handle SA2UL_open ( uint32_t  index,
const SA2UL_Params params 
)

This function opens a given SA2UL module.

Parameters
indexIndex of config to use in the SA2UL_Config array
paramsPointer to open parameters. If NULL is passed, then default values will be used
Returns
A SA2UL_Handle on success or a NULL on an error or if it has been opened already

◆ SA2UL_close()

void SA2UL_close ( SA2UL_Handle  handle)

Function to close a SA2UL module specified by the SA2UL handle.

Parameters
handleSA2UL_Handle returned from SA2UL_open()

◆ SA2UL_contextAlloc()

int32_t SA2UL_contextAlloc ( SA2UL_Handle  handle,
SA2UL_ContextObject ctxObj,
const SA2UL_ContextParams ctxPrms 
)

Function to configure secure context.

Parameters
handleSA2UL_Handle returned from SA2UL_open()
ctxObjPointer to SA2UL_ContextObject structure
ctxPrmsPointer to secure context parameters.If NULL is passed, then default values will be used
Returns
A SystemP_SUCCESS on success or a NULL on an error or if the instance index has NOT been opened yet

◆ SA2UL_contextFree()

int32_t SA2UL_contextFree ( SA2UL_ContextObject pCtxObj)

Function to free secure context configuration.

Parameters
pCtxObjPointer to SA2UL_ContextObject structure
Returns
A SystemP_SUCCESS on success or a NULL on an error or if the instance index has NOT been opened yet

◆ SA2UL_contextProcess()

int32_t SA2UL_contextProcess ( SA2UL_ContextObject ctxObj,
const uint8_t *  input,
uint32_t  ilen,
uint8_t *  output 
)

Function to transfer and recieve data buffer.

Parameters
ctxObjPointer to SA2UL_ContextObject structure
inputPointer to input buffer to be processed
ilenLength of the input buffer
outputPointer to output buffer after the process is complete
Returns
A SystemP_SUCCESS on success or a NULL on an error or if the instance index has NOT been opened yet

◆ SA2UL_Params_init()

static void SA2UL_Params_init ( SA2UL_Params prms)
inlinestatic

Function to initialize default SA2UL parameters.

Parameters
prmsPointer to open parameters.

◆ SA2UL_rngSetup()

int32_t SA2UL_rngSetup ( SA2UL_Handle  handle)

setup the SA2UL RNG module.

Parameters
handleSA2UL_Handle returned from SA2UL_open()
Returns
SystemP_SUCCESS if successful

◆ SA2UL_rngRead()

int32_t SA2UL_rngRead ( SA2UL_Handle  handle,
uint32_t *  out 
)

Read random numbers into the output buffer.

Parameters
handleSA2UL_Handle returned from SA2UL_open()
outpointer to the buffer for the 128 bit random data.
Returns
returns SystemP_SUCCESS if requested data is available. SystemP_FAILURE if RNG is not initialized.

◆ SA2UL_ContextParams_init()

static void SA2UL_ContextParams_init ( SA2UL_ContextParams ctxPrms)
inlinestatic

Variable Documentation

◆ gSa2ulConfig

SA2UL_Config gSa2ulConfig[]
extern

Externally defined driver configuration array.

◆ gSa2ulConfigNum

uint32_t gSa2ulConfigNum
extern

Externally defined driver configuration Num.