AM243x MCU+ SDK  08.05.00

Introduction

Functions

tLegStates PN_getLegState (void)
 Returns the IRT Legacy mode state. More...
 
void PN_setLegState (void *arg, void *arg2)
 Sets the state of legacy state machine This API is registered as a callback in PN_registerSetState. More...
 
void PN_setLegPkt (void *arg, void *arg2)
 Sets the Ethernet packet to output during legacy startup Usually a copy of RTC3 PPM. This API is registered as a callback in PN_registerSetPkt. More...
 
void PN_registerSetState (PN_Handle pnHandle, pnLegCallBack_t callBack)
 Registers callback function for legacy state This callback is used to change the Legacy state machine. More...
 
void PN_registerSetPkt (PN_Handle pnHandle, pnLegCallBack_t callBack)
 Registers callback function for packet pointer This callback is used to configure the packet send by the IRT state machine. More...
 

Typedefs

typedef void(* pnLegCallBack_t) (void *arg, void *arg2)
 Callback function for processing Profinet IRQs. More...
 

Enumerations

enum  tLegStates { NOINIT, READY, SENDPPM, ABORT }
 possible states for legacy suppport state machine More...
 

Typedef Documentation

◆ pnLegCallBack_t

typedef void(* pnLegCallBack_t) (void *arg, void *arg2)

Callback function for processing Profinet IRQs.

Parameters
arg
arg2
Precondition
IRT_LEGACY_STARTUP_SUPPORT defined

Enumeration Type Documentation

◆ tLegStates

enum tLegStates

possible states for legacy suppport state machine

Precondition
IRT_LEGACY_STARTUP_SUPPORT defined
Enumerator
NOINIT 

not initialized yet

READY 

initialized

SENDPPM 

sending RTC3 packet in green at RR=128

ABORT 

error case

Function Documentation

◆ PN_getLegState()

tLegStates PN_getLegState ( void  )

Returns the IRT Legacy mode state.

Returns
Current state of the Legacy mode state machine

◆ PN_setLegState()

void PN_setLegState ( void *  arg,
void *  arg2 
)

Sets the state of legacy state machine This API is registered as a callback in PN_registerSetState.

Parameters
argnew state tLegStates
arg2not used

◆ PN_setLegPkt()

void PN_setLegPkt ( void *  arg,
void *  arg2 
)

Sets the Ethernet packet to output during legacy startup Usually a copy of RTC3 PPM. This API is registered as a callback in PN_registerSetPkt.

Parameters
argPointer to valid packet buffer, no checks. t_rtcPacket
arg2not used

◆ PN_registerSetState()

void PN_registerSetState ( PN_Handle  pnHandle,
pnLegCallBack_t  callBack 
)

Registers callback function for legacy state This callback is used to change the Legacy state machine.

Parameters
pnHandleProfinet Handle
[in]callBackCallback function pointer
Precondition
IRT_LEGACY_STARTUP_SUPPORT defined

◆ PN_registerSetPkt()

void PN_registerSetPkt ( PN_Handle  pnHandle,
pnLegCallBack_t  callBack 
)

Registers callback function for packet pointer This callback is used to configure the packet send by the IRT state machine.

Parameters
pnHandleProfinet Handle
[in]callBackCallback function pointer
Precondition
IRT_LEGACY_STARTUP_SUPPORT defined