AM243x MCU+ SDK  08.05.00

Introduction

This module contains APIs to program and use DMA drivers available in the SoC with MCSPI.

Data Structures

struct  MCSPI_DmaFxns
 Driver implementation callbacks. More...
 
struct  MCSPI_DmaConfig
 MCSPI DMA Configuration, these are filled by SysCfg based on the DMA driver that is selected. More...
 

Functions

MCSPI_DmaHandle MCSPI_dmaOpen (int32_t index)
 API to open an MCSPI DMA channel. More...
 
int32_t MCSPI_dmaClose (MCSPI_Handle handle, const MCSPI_ChConfig *chCfg)
 API to close an MCSPI DMA channel. More...
 
int32_t MCSPI_dmaChInit (MCSPI_Handle handle, const MCSPI_ChConfig *chCfg, const MCSPI_DmaChConfig *dmaChCfg)
 API to init a DMA Channel opened. More...
 
int32_t MCSPI_dmaTransfer (MCSPI_Object *obj, MCSPI_ChObject *chObj, const MCSPI_Attrs *attrs, MCSPI_Transaction *transaction)
 API to do a DMA transfer using a specific DMA driver - UDMA, EDMA etc. More...
 
int32_t MCSPI_dmaStop (MCSPI_Object *obj, const MCSPI_Attrs *attrs, MCSPI_ChObject *chObj, uint32_t chNum)
 API to Stop DMA using a specific DMA driver - UDMA, EDMA etc. More...
 

Typedefs

typedef void * MCSPI_DmaHandle
 Handle to the MCSPI DMA Config Object returned by MCSPI_dmaOpen. More...
 
typedef int32_t(* MCSPI_dmaOpenFxn) (void *mcspiDmaArgs)
 Driver implementation to open a specific DMA driver channel - UDMA, EDMA etc. More...
 
typedef int32_t(* MCSPI_dmaCloseFxn) (MCSPI_Handle handle, const MCSPI_ChConfig *chCfg)
 Driver implementation to close a specific DMA driver channel - UDMA, EDMA etc. More...
 
typedef int32_t(* MCSPI_dmaChInitFxn) (MCSPI_Handle handle, const MCSPI_ChConfig *chCfg, const MCSPI_DmaChConfig *dmaChCfg)
 Driver implementation to init a DMA channel params using a specific DMA driver - UDMA, EDMA etc. More...
 
typedef int32_t(* MCSPI_dmaTransferMasterFxn) (MCSPI_Object *obj, MCSPI_ChObject *chObj, const MCSPI_Attrs *attrs, MCSPI_Transaction *transaction)
 Driver implementation to do a DMA transfer using a specific DMA driver - UDMA, EDMA etc. More...
 
typedef int32_t(* MCSPI_dmaStopFxn) (MCSPI_Object *obj, const MCSPI_Attrs *attrs, MCSPI_ChObject *chObj, uint32_t chNum)
 Driver implementation to Stop DMA using a specific DMA driver - UDMA, EDMA etc. More...
 

Typedef Documentation

◆ MCSPI_DmaHandle

typedef void* MCSPI_DmaHandle

Handle to the MCSPI DMA Config Object returned by MCSPI_dmaOpen.

◆ MCSPI_dmaOpenFxn

typedef int32_t(* MCSPI_dmaOpenFxn) (void *mcspiDmaArgs)

Driver implementation to open a specific DMA driver channel - UDMA, EDMA etc.

Typically this callback is hidden from the end application and is implemented when a new DMA driver needs to be supported.

Parameters
mcspiDmaArgs[in] DMA specific arguments, obtained from the config
Returns
SystemP_SUCCESS on success, else failure

◆ MCSPI_dmaCloseFxn

typedef int32_t(* MCSPI_dmaCloseFxn) (MCSPI_Handle handle, const MCSPI_ChConfig *chCfg)

Driver implementation to close a specific DMA driver channel - UDMA, EDMA etc.

Typically this callback is hidden from the end application and is implemented when a new DMA driver needs to be supported.

Parameters
MCSPI_DmaHandle[in] MCSPI DMA Object handle returned from MCSPI_dmaOpen
mcspiDmaArgs[in] DMA specific arguments, obtained from the config
Returns
SystemP_SUCCESS on success, else failure

◆ MCSPI_dmaChInitFxn

typedef int32_t(* MCSPI_dmaChInitFxn) (MCSPI_Handle handle, const MCSPI_ChConfig *chCfg, const MCSPI_DmaChConfig *dmaChCfg)

Driver implementation to init a DMA channel params using a specific DMA driver - UDMA, EDMA etc.

Typically this callback is hidden from the end application and is implemented when a new DMA driver needs to be supported.

Parameters
handle[in] MCSPI_Handle returned from MCSPI_open()
chCfg[in] Pointer to MCSPI_ChConfig. This parameter can't be NULL
dmaChCfg[in] Pointer to MCSPI_DmaChConfig. This parameter can't be NULL
Returns
SystemP_SUCCESS on success, else failure

◆ MCSPI_dmaTransferMasterFxn

typedef int32_t(* MCSPI_dmaTransferMasterFxn) (MCSPI_Object *obj, MCSPI_ChObject *chObj, const MCSPI_Attrs *attrs, MCSPI_Transaction *transaction)

Driver implementation to do a DMA transfer using a specific DMA driver - UDMA, EDMA etc.

Typically this callback is hidden from the end application and is implemented when a new DMA driver needs to be supported.

Parameters
obj[in] Pointer to MCSPI object
chObj[in] Pointer to MCSPI_ChObject. This parameter can't be NULL
attrs[in] Pointer to MCSPI_Attrs. This parameter can't be NULL
transaction[in] Pointer to MCSPI_Transaction. This parameter can't be NULL
Returns
SystemP_SUCCESS on success, else failure

◆ MCSPI_dmaStopFxn

typedef int32_t(* MCSPI_dmaStopFxn) (MCSPI_Object *obj, const MCSPI_Attrs *attrs, MCSPI_ChObject *chObj, uint32_t chNum)

Driver implementation to Stop DMA using a specific DMA driver - UDMA, EDMA etc.

Typically this callback is hidden from the end application and is implemented when a new DMA driver needs to be supported.

Parameters
obj[in] Pointer to MCSPI object
attrs[in] Pointer to MCSPI_Attrs. This parameter can't be NULL
chObj[in] Pointer to MCSPI_ChObject. This parameter can't be NULL
chNum[in] Channel number
Returns
SystemP_SUCCESS on success, else failure

Function Documentation

◆ MCSPI_dmaOpen()

MCSPI_DmaHandle MCSPI_dmaOpen ( int32_t  index)

API to open an MCSPI DMA channel.

This API will open a DMA Channel using the appropriate DMA driver callbacks and the registered via Sysconfig

Parameters
index[in] Index of the DMA Config selected for this particular MCSPI driver instance
Returns
Handle to the MCSPI DMA Config Object

◆ MCSPI_dmaClose()

int32_t MCSPI_dmaClose ( MCSPI_Handle  handle,
const MCSPI_ChConfig chCfg 
)

API to close an MCSPI DMA channel.

This API will open a DMA Channel using the appropriate DMA driver callbacks registered via Sysconfig

Parameters
handle[in] MCSPI_Handle returned from MCSPI_open()
chCfg[in] Pointer to MCSPI_ChConfig. This parameter can't be NULL
Returns
SystemP_SUCCESS on success, else failure

◆ MCSPI_dmaChInit()

int32_t MCSPI_dmaChInit ( MCSPI_Handle  handle,
const MCSPI_ChConfig chCfg,
const MCSPI_DmaChConfig dmaChCfg 
)

API to init a DMA Channel opened.

This API will open a DMA Channel using the appropriate DMA driver callbacks registered via Sysconfig

Parameters
handle[in] MCSPI_Handle returned from MCSPI_open()
chCfg[in] Pointer to MCSPI_ChConfig. This parameter can't be NULL
dmaChCfg[in] Pointer to MCSPI_DmaChConfig. This parameter can't be NULL
Returns
SystemP_SUCCESS on success, else failure

◆ MCSPI_dmaTransfer()

int32_t MCSPI_dmaTransfer ( MCSPI_Object obj,
MCSPI_ChObject chObj,
const MCSPI_Attrs attrs,
MCSPI_Transaction transaction 
)

API to do a DMA transfer using a specific DMA driver - UDMA, EDMA etc.

Typically this callback is hidden from the end application and is implemented when a new DMA driver needs to be supported.

Parameters
obj[in] Pointer to MCSPI object
chObj[in] Pointer to MCSPI_ChObject. This parameter can't be NULL
attrs[in] Pointer to MCSPI_Attrs. This parameter can't be NULL
transaction[in] Pointer to MCSPI_Transaction. This parameter can't be NULL
Returns
SystemP_SUCCESS on success, else failure

◆ MCSPI_dmaStop()

int32_t MCSPI_dmaStop ( MCSPI_Object obj,
const MCSPI_Attrs attrs,
MCSPI_ChObject chObj,
uint32_t  chNum 
)

API to Stop DMA using a specific DMA driver - UDMA, EDMA etc.

Typically this callback is hidden from the end application and is implemented when a new DMA driver needs to be supported.

Parameters
obj[in] Pointer to MCSPI object
attrs[in] Pointer to MCSPI_Attrs. This parameter can't be NULL
chObj[in] Pointer to MCSPI_ChObject. This parameter can't be NULL
chNum[in] Channel number
Returns
SystemP_SUCCESS on success, else failure