AM243x MCU+ SDK  08.05.00

Introduction

The CPSW MAC port module provides additional IOCTL commands than those supported by the generic Enet MAC Port API set.

CPSW MAC port clocks:

Features:

Compile-time configuration:

Data Structures

struct  CpswMacPort_TxShortIpgCfg
 Configuration of transmit short inter packet gap feature. More...
 
struct  CpswMacPort_PortTxShortIpgCfg
 MAC port's short gap configuration. More...
 
struct  CpswMacPort_InterVlanRoutingCfg
 Port interVLAN configuration parameters. More...
 
struct  CpswMacPort_FifoStats
 FIFO related statistics of a MAC port. More...
 
struct  CpswMacPort_IpTsCfg
 Port IP configuration for time synchronization events. More...
 
struct  CpswMacPort_TsEventCfg
 Port configuration for time synchronization. More...
 
struct  CpswMacPort_EnableTsEventInArgs
 Input args for CPSW_MACPORT_IOCTL_ENABLE_CPTS_EVENT. More...
 
struct  CpswMacPort_EstTimestampCfg
 EST timestamping configuration parameters. More...
 
struct  CpswMacPort_Cfg
 MAC port module configuration parameters. More...
 

Functions

void CpswMacPort_initCfg (CpswMacPort_Cfg *macPortCfg)
 Initialize CPSW MAC port configuration parameters. More...
 

Enumerations

enum  CpswMacPort_Ioctl {
  CPSW_MACPORT_IOCTL_GET_FIFO_STATS = CPSW_MACPORT_PUBLIC_IOCTL(0U), CPSW_MACPORT_IOCTL_ENABLE_CPTS_EVENT = CPSW_MACPORT_PUBLIC_IOCTL(1U), CPSW_MACPORT_IOCTL_DISABLE_CPTS_EVENT = CPSW_MACPORT_PUBLIC_IOCTL(2U), CPSW_MACPORT_IOCTL_EST_ENABLE_TIMESTAMP = CPSW_MACPORT_PUBLIC_IOCTL(3U),
  CPSW_MACPORT_IOCTL_EST_DISABLE_TIMESTAMP = CPSW_MACPORT_PUBLIC_IOCTL(4U)
}
 CPSW MAC port IOCTL commands. More...
 
enum  CpswMacPort_InterVlanRouteId {
  CPSW_MACPORT_INTERVLAN_ROUTEID_FIRST, CPSW_MACPORT_INTERVLAN_ROUTEID_1 = CPSW_MACPORT_INTERVLAN_ROUTEID_FIRST, CPSW_MACPORT_INTERVLAN_ROUTEID_2, CPSW_MACPORT_INTERVLAN_ROUTEID_3,
  CPSW_MACPORT_INTERVLAN_ROUTEID_4, CPSW_MACPORT_INTERVLAN_ROUTEID_LAST = CPSW_MACPORT_INTERVLAN_ROUTEID_4
}
 MAC port interVLAN route identifier. More...
 
enum  CpswMacPort_EstTimestampMode { CPSW_MACPORT_EST_TIMESTAMP_ALL, CPSW_MACPORT_EST_TIMESTAMP_ONEPRI, CPSW_MACPORT_EST_TIMESTAMP_FIRST, CPSW_MACPORT_EST_TIMESTAMP_FIRST_ONEPRI }
 EST timestamping modes. More...
 

Macros

#define CPSW_MACPORT_PUBLIC_IOCTL(x)
 Helper macro to create IOCTL commands for CPSW MAC port module. More...
 
#define CPSW_MACPORT_EST_TIME_INTERVAL_MIN   (0x010U)
 EST non-zero minimum time interval, in wireside clocks. Needed to guarantee that next fetch value has time to be fetched before current fetch count is over. More...
 
#define CPSW_MACPORT_EST_TIME_INTERVAL_MAX   (0x3FFFU)
 EST maximum time interval (14-bit), in wireside clocks. More...
 
#define CPSW_MACPORT_EST_TIME_STEP_1G   (8U)
 Time interval step in nsecs for 1 Gbps link. More...
 
#define CPSW_MACPORT_EST_TIME_STEP_100M   (40U)
 Time interval step in nsecs for 100 Mbps link. More...
 
#define CPSW_MACPORT_EST_TIME_STEP_10M   (400U)
 Time interval step in nsecs for a 10 Mbps link. More...
 
#define CPSW_MACPORT_EST_TIME_MIN(speed)   (CPSW_MACPORT_EST_TIME_STEP_##speed * CPSW_MACPORT_EST_TIME_INTERVAL_MIN)
 Min time interval in nsecs for given link speed. More...
 
#define CPSW_MACPORT_EST_TIME_MAX(speed)   (CPSW_MACPORT_EST_TIME_STEP_##speed * CPSW_MACPORT_EST_TIME_INTERVAL_MAX)
 Max time interval in nsecs for given link speed. More...
 
#define CPSW_MACPORT_EST_ALLOWCNT_FACTOR_1G   (1U)
 EST allow count scaling factor for 1 Gbps link. More...
 
#define CPSW_MACPORT_EST_ALLOWCNT_FACTOR_100M   (2U)
 EST allow count scaling factor for 100 Mbps link. More...
 
#define CPSW_MACPORT_EST_ALLOWCNT_FACTOR_10M   (2U)
 EST allow count scaling factor for 10 Mbps link. More...
 
#define CPSW_MACPORT_EST_GUARD_BAND(maxPktSize, speed)
 Guard band duration in nsecs for given link speed and maximum packet size in previous time interval. More...
 

Macro Definition Documentation

◆ CPSW_MACPORT_PUBLIC_IOCTL

#define CPSW_MACPORT_PUBLIC_IOCTL (   x)
Value:
ENET_IOCTL_MACPORT_BASE | \
ENET_IOCTL_PER_CPSW | \
ENET_IOCTL_MIN(x))

Helper macro to create IOCTL commands for CPSW MAC port module.

◆ CPSW_MACPORT_EST_TIME_INTERVAL_MIN

#define CPSW_MACPORT_EST_TIME_INTERVAL_MIN   (0x010U)

EST non-zero minimum time interval, in wireside clocks. Needed to guarantee that next fetch value has time to be fetched before current fetch count is over.

◆ CPSW_MACPORT_EST_TIME_INTERVAL_MAX

#define CPSW_MACPORT_EST_TIME_INTERVAL_MAX   (0x3FFFU)

EST maximum time interval (14-bit), in wireside clocks.

◆ CPSW_MACPORT_EST_TIME_STEP_1G

#define CPSW_MACPORT_EST_TIME_STEP_1G   (8U)

Time interval step in nsecs for 1 Gbps link.

◆ CPSW_MACPORT_EST_TIME_STEP_100M

#define CPSW_MACPORT_EST_TIME_STEP_100M   (40U)

Time interval step in nsecs for 100 Mbps link.

◆ CPSW_MACPORT_EST_TIME_STEP_10M

#define CPSW_MACPORT_EST_TIME_STEP_10M   (400U)

Time interval step in nsecs for a 10 Mbps link.

◆ CPSW_MACPORT_EST_TIME_MIN

#define CPSW_MACPORT_EST_TIME_MIN (   speed)    (CPSW_MACPORT_EST_TIME_STEP_##speed * CPSW_MACPORT_EST_TIME_INTERVAL_MIN)

Min time interval in nsecs for given link speed.

◆ CPSW_MACPORT_EST_TIME_MAX

#define CPSW_MACPORT_EST_TIME_MAX (   speed)    (CPSW_MACPORT_EST_TIME_STEP_##speed * CPSW_MACPORT_EST_TIME_INTERVAL_MAX)

Max time interval in nsecs for given link speed.

◆ CPSW_MACPORT_EST_ALLOWCNT_FACTOR_1G

#define CPSW_MACPORT_EST_ALLOWCNT_FACTOR_1G   (1U)

EST allow count scaling factor for 1 Gbps link.

◆ CPSW_MACPORT_EST_ALLOWCNT_FACTOR_100M

#define CPSW_MACPORT_EST_ALLOWCNT_FACTOR_100M   (2U)

EST allow count scaling factor for 100 Mbps link.

◆ CPSW_MACPORT_EST_ALLOWCNT_FACTOR_10M

#define CPSW_MACPORT_EST_ALLOWCNT_FACTOR_10M   (2U)

EST allow count scaling factor for 10 Mbps link.

◆ CPSW_MACPORT_EST_GUARD_BAND

#define CPSW_MACPORT_EST_GUARD_BAND (   maxPktSize,
  speed 
)
Value:
(((((maxPktSize) + 4U) * \
CPSW_MACPORT_EST_ALLOWCNT_FACTOR_##speed) + 292U) * \
CPSW_MACPORT_EST_TIME_STEP_##speed)

Guard band duration in nsecs for given link speed and maximum packet size in previous time interval.

Enumeration Type Documentation

◆ CpswMacPort_Ioctl

CPSW MAC port IOCTL commands.

Enumerator
CPSW_MACPORT_IOCTL_GET_FIFO_STATS 

Get MAC port FIFO statistics.

IOCTL parameters:

CPSW_MACPORT_IOCTL_ENABLE_CPTS_EVENT 

Enable Ethernet port CPTS event.

IOCTL parameters:

CPSW_MACPORT_IOCTL_DISABLE_CPTS_EVENT 

Disable Ethernet port CPTS event.

IOCTL parameters:

CPSW_MACPORT_IOCTL_EST_ENABLE_TIMESTAMP 

Enable EST packet timestamping functionality.

Once enabled, timestamps can be retrieved using CPSW CPTS IOCTLs.

IOCTL parameters: inArgs: CpswMacPort_EstTimestampCfg outArgs: None

CPSW_MACPORT_IOCTL_EST_DISABLE_TIMESTAMP 

Disable EST packet timestamping functionality.

IOCTL parameters: inArgs: EnetMacPort_GenericInArgs outArgs: None

◆ CpswMacPort_InterVlanRouteId

MAC port interVLAN route identifier.

Enumerator
CPSW_MACPORT_INTERVLAN_ROUTEID_FIRST 

First interVLAN route Id

CPSW_MACPORT_INTERVLAN_ROUTEID_1 

InterVLAN route Id 1

CPSW_MACPORT_INTERVLAN_ROUTEID_2 

InterVLAN route Id 2

CPSW_MACPORT_INTERVLAN_ROUTEID_3 

InterVLAN route Id 3

CPSW_MACPORT_INTERVLAN_ROUTEID_4 

InterVLAN route Id 4

CPSW_MACPORT_INTERVLAN_ROUTEID_LAST 

Last interVLAN route Id

◆ CpswMacPort_EstTimestampMode

EST timestamping modes.

Enumerator
CPSW_MACPORT_EST_TIMESTAMP_ALL 

Timestamp all express packets on any priority.

CPSW_MACPORT_EST_TIMESTAMP_ONEPRI 

Timestamp only express packets of a given priority.

CPSW_MACPORT_EST_TIMESTAMP_FIRST 

Timestamp the first express packet in each time interval.

CPSW_MACPORT_EST_TIMESTAMP_FIRST_ONEPRI 

Timestamp the first express packet of a given priority in the time interval.

Function Documentation

◆ CpswMacPort_initCfg()

void CpswMacPort_initCfg ( CpswMacPort_Cfg macPortCfg)

Initialize CPSW MAC port configuration parameters.

Parameters
macPortCfgConfiguration parameters to be initialized
ENET_IOCTL_TYPE_PUBLIC
@ ENET_IOCTL_TYPE_PUBLIC
Definition: enet_ioctl.h:209