Go to the source code of this file.
Functions | |
void | CycleCounterP_init (const uint64_t cpuFreqHz) |
initialize PMU Cycle Counter More... | |
uint32_t | CycleCounterP_getCount32 () |
Get 32b CPU cycle counter value. More... | |
void | CycleCounterP_reset () |
Enable, reset, clear overflow for CPU cycle counter. More... | |
uint64_t | CycleCounterP_getCount64 () |
Get 64b CPU cycle counter value. More... | |
uint64_t | CycleCounterP_nsToTicks (const uint64_t nanosecs) |
API function to convert nanosecs to PMU counter ticks. More... | |