Data Storage API.
Functions | |
IOL_FUNC_DECL IOL_EErrorInfo | IOLM_API_DS_eSet (INT8U u8Port_p, IOLM_EDSActivationState eActState_p, IOLM_EDSMode eMode_p) |
Setup Data Storage mode. More... | |
IOL_FUNC_DECL IOL_EErrorInfo | IOLM_API_DS_eDelete (INT8U u8Port_p) |
Delete Data Storage content. More... | |
IOL_FUNC_DECL IOL_EErrorInfo IOLM_API_DS_eDelete | ( | INT8U | u8Port_p | ) |
Delete Data Storage content.
The Data Storage content is marked as invalid and the non volatile memory will be cleared. This function can be called if no Data Storage activity is pending.
[in] | u8Port_p | The port number of the affected port. |
IOL_FUNC_DECL IOL_EErrorInfo IOLM_API_DS_eSet | ( | INT8U | u8Port_p, |
IOLM_EDSActivationState | eActState_p, | ||
IOLM_EDSMode | eMode_p | ||
) |
Setup Data Storage mode.
Data Storage set function is used to enable or disable the DS activity for a specific port. The function can be called every time if no DS action is pending. If the Data Storage is enabled it starts immediately to download/upload data.
[in] | u8Port_p | The port number of the affected port. |
[in] | eActState_p | State of DS (see IOLM_EDSActivationState). |
[in] | eMode_p | Mode of DS (see IOLM_EDSMode). |