Definition for ConnectionManager callback functions. More...
#include <EI_API_def.h>
Data Fields | |
uint8_t | prioTimeTick |
uint8_t | timeOutTicks |
uint32_t | o2tNwConId |
uint32_t | t2oNwConId |
uint16_t | conSerialNum |
uint16_t | orgVendorId |
uint32_t | orgSerialNum |
uint8_t | timeOutMulti |
uint32_t | o2tRPI |
uint32_t | o2tConPara |
uint32_t | t2oRPI |
uint16_t | t2oConPara |
uint8_t | typeTrigger |
uint8_t | conPathSize |
uint8_t | conPath [80] |
Definition for ConnectionManager callback functions.
Information from the ForwardOpen, LargeForwardOpen or ForwardClose message