EtherNet/IP™ Adapter  1.04.10
User Reference Manual

◆ EI_API_CIP_NODE_delete()

uint32_t EI_API_CIP_NODE_delete ( T pCipNode_p)

Delete the CIP node specified by parameter pCipNode_p.

If a CIP node was created it can be deleted with this function. The memory which was allocated by the CIP node will be freed.

Parameters
[in]pCipNode_pPointer to the CIP node.
Returns
EI_API_CIP_EError_t as uint32_t value.
Return values
EI_API_CIP_eERR_OKSuccess.
EI_API_CIP_eERR_NODE_INVALIDCIP node is invalid, possibly EI_API_CIP_NODE_new() was not called.
Example
#include <api/EI_API.h>
EI_API_CIP_NODE_T* pEI_API_CIP_NODE = NULL;
uint32_t errCode;
// create a CIP node
pEI_API_CIP_NODE = EI_API_CIP_NODE_new();
...
// delete CIP node
errCode = EI_API_CIP_NODE_delete(pEI_API_CIP_NODE);
See also
EI_API_CIP_NODE_new
EI_API_CIP_NODE_delete
ETHIP_API uint32_t EI_API_CIP_NODE_delete(T *pCipNode_p)
Delete the CIP node specified by parameter pCipNode_p.
Definition: EI_API_CIP_main.c:153
EI_API_CIP_NODE_new
ETHIP_API T * EI_API_CIP_NODE_new(void)
Create a new CIP node.
Definition: EI_API_CIP_main.c:68