uint32_t EI_API_ADP_setEnipAcdAddr | ( | T * | pAdp_p, |
const EI_API_ADP_SParam_t * | pEnipAcdAddr_p | ||
) |
Set the address conflict detection MAC address (Instance Attribute ID: 11).
Function that sets the MAC address of the last address conflict detected by the Address Conflict Detection (ACD).
[in] | pAdp_p | Pointer to the adapter. |
[in] | pEnipAcdAddr_p | Pointer to the Ethernet Address Conflict Detection MAC address packed within a EI_API_ADP_SParam_t type. |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |
EI_API_ADP_eERR_LENGTH | Illegal parameter length. |