uint32_t EI_API_ADP_getConfigurationControl | ( | T * | pAdp_p, |
EIP_SConfigurationControl_t * | pConfigurationControl_p | ||
) |
Get the current configuration control setting (Instance Attribute ID: 3).
This function gets the configuration control setting of the TCP/IP object attribute 3.
[in] | pAdp_p | Pointer to the adapter. |
[out] | pConfigurationControl_p | Pointer to the configuration control struct. |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |