uint32_t EI_API_ADP_getDHCP | ( | T * | pAdp_p, |
bool * | pDhcpEnabled_p | ||
) |
Get the current DHCP setting (Instance Attribute ID: 3).
This function returns directly the DHCP flag in the return value.
[in] | pAdp_p | Pointer to the adapter. |
[out] | pDhcpEnabled_p | Pointer to a boolean that is set to true if DHCP is enabled and false if not. |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |