uint32_t EI_API_ADP_getRevision | ( | T * | pAdp_p, |
EI_API_ADP_SRevision_t * | pRevision_p | ||
) |
Get the adapter Revision (Instance Attribute ID: 4).
Function that returns the revision of the adapter selected by parameter pAdp_p
. The revision attribute is divided into major and minor revision number.
[in] | pAdp_p | Pointer to the adapter. |
[out] | pRevision_p | Pointer to an adapter revision structure. |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |