uint32_t EI_API_ADP_setSerialNumber | ( | T * | pAdp_p, |
uint32_t | serialNumber_p | ||
) |
Set the adapter's unique Serial Number (Instance Attribute ID: 6).
Function to set a unique serial number of the adapter selected by parameter pAdp_p
. This attribute is used in conjunction with the vendor ID to form a unique identifier for each device on any CIP network. It is in the responsibility of the device vendor to guarantee that the serial number is unique across all of the vendor's devices.
The value zero is not a valid serial number and shall not be assigned to a product.
[in] | pAdp_p | Pointer to the adapter. |
[in] | serialNumber_p | New serial number. |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |