uint32_t EI_API_ADP_delete | ( | T * | pAdp_p | ) |
Delete an existing EtherNet/IP adapter.
If an adapter was created it can be deleted with this function. The memory which was allocated by the adapter will be freed.
[in] | pAdp_p | Pointer to the adapter. |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |