uint32_t EC_API_SLV_CoE_getObjectEntryCount | ( | EC_API_SLV_SHandle_t * | pEcSlaveApi_p, |
EC_API_SLV_SCoE_Object_t * | pObject_p, | ||
uint8_t * | pCount_p | ||
) |
This function returns the number of entries of a object.
Returns the number of entries of an object
[in] | pEcSlaveApi_p | The pointer to the EtherCAT API instance. |
[in] | pObject_p | Pointer to the object instance. |
[out] | pCount_p | Number of entries of the object. |