void EC_API_SLV_FoE_cbRegisterCloseFileHandler | ( | EC_API_SLV_SHandle_t * | pEcSlaveApi_p, |
void * | pContext_p, | ||
EC_API_SLV_FoE_CBCloseFileHandler_t | cbFunc_p | ||
) |
This is the function to register FoE close function.
This function registers a function pointer which must be implemented by the user. The user defined function will be called if a file read or write request is received from the master.
[in] | pEcSlaveApi_p | The pointer to the EtherCAT API instance. |
[in] | pContext_p | closeFileHandler call context |
[in] | cbFunc_p | cbFunc Function pointer to the FoE Close file Handler |