void EC_API_SLV_cbRegisterPreSeqInputPDBuffer | ( | EC_API_SLV_SHandle_t * | pEcSlaveApi_p, |
void * | pContext_p, | ||
EC_API_SLV_CBPreSeqInputPD_t | cbFunc_p | ||
) |
This is the function to register a function which gets an external Process data buffer.
[in] | pEcSlaveApi_p | The pointer to the EtherCAT API instance. |
[in] | pContext_p | PreSeqInputPDBuffer callback context |
[in] | cbFunc_p | Function pointer to the Input Process data Handler |