AM243x MCU+ SDK  08.04.00
Pcie_DeviceCfgBaseAddr Struct Reference

Detailed Description

The Pcie_DeviceCfg is used to specify device level configuration of the driver instance.

Data Fields

void * cfgBase
 
void * dataBase
 
uint32_t dataReserved
 
void * devParams
 

Field Documentation

◆ cfgBase

void* Pcie_DeviceCfgBaseAddr::cfgBase

Device-dependant configuration base address.

◆ dataBase

void* Pcie_DeviceCfgBaseAddr::dataBase

Base address of the "data" area (remote device memory)

◆ dataReserved

uint32_t Pcie_DeviceCfgBaseAddr::dataReserved

Reserved part of real data area due to memory mapping.

◆ devParams

void* Pcie_DeviceCfgBaseAddr::devParams

Driver version-dependant device params. Not all HW will have these (put NULL).