AM243x MCU+ SDK  08.04.00

Detailed Description

Input args for CPSW_ALE_IOCTL_SET_PORT_MIRROR_CFG command.

Data Fields

bool srcEn
 
bool dstEnEn
 
bool matchEn
 
uint32_t dstPortNum
 
uint32_t toPortNum
 
CpswAle_MirrorMatchParams matchParams
 
uint32_t srcPortNumMask
 

Field Documentation

◆ srcEn

bool CpswAle_PortMirroringCfg::srcEn

Enables the source port mirror option. When this bit is set any port with the pX_mirror_sp set in the ALE Port Control registers set will have its received traffic also sent to the mirror_top port

◆ dstEnEn

bool CpswAle_PortMirroringCfg::dstEnEn

Enables the destination port mirror option. When this bit is set any traffic destined for the mirror_dp port will have its transmit traffic also sent to the mirror_top port

◆ matchEn

bool CpswAle_PortMirroringCfg::matchEn

Enables the match mirror option. When this bit is set any traffic whose destination, source, VLAN or OUI matches the mirror_midx entry index will have that traffic also sent to the mirror_top port

◆ dstPortNum

uint32_t CpswAle_PortMirroringCfg::dstPortNum

The port to which destination traffic destined will be duplicated

◆ toPortNum

uint32_t CpswAle_PortMirroringCfg::toPortNum

The destination port for the mirror traffic

◆ matchParams

CpswAle_MirrorMatchParams CpswAle_PortMirroringCfg::matchParams

ALE lookup table entry info that when a match occurs will cause this traffic to be mirrored to the mirror_top port. Must be valid if matchEn is TRUE

◆ srcPortNumMask

uint32_t CpswAle_PortMirroringCfg::srcPortNumMask

Source port number mirroring enable bitmask