AM243x MCU+ SDK  08.04.00
sciclient_soc_priv.c File Reference

Functions

uint32_t Sciclient_getContext (uint32_t contextType, uint32_t coreId)
 API to get the right core context. More...
 
uint32_t Sciclient_getDevId (uint32_t coreId)
 

Variables

CSL_SecProxyCfg gSciclientSecProxyCfg
 This structure contains configuration parameters for the sec_proxy IP. More...
 

Function Documentation

◆ Sciclient_getContext()

uint32_t Sciclient_getContext ( uint32_t  contextType,
uint32_t  coreId 
)

API to get the right core context.

Parameters
contextTypeContext type(Secure or Non Secure).
coreIdID of the Core on which the driver is running
Returns
context Context found.

◆ Sciclient_getDevId()

uint32_t Sciclient_getDevId ( uint32_t  coreId)

Variable Documentation

◆ gSciclientSecProxyCfg

CSL_SecProxyCfg gSciclientSecProxyCfg
Initial value:
=
{
(CSL_sec_proxyRegs *)CSL_DMASS0_SEC_PROXY_MMRS_BASE,
(CSL_sec_proxy_scfgRegs *)CSL_DMASS0_SEC_PROXY_SCFG_BASE,
(CSL_sec_proxy_rtRegs *)CSL_DMASS0_SEC_PROXY_RT_BASE,
(uint64_t)CSL_DMASS0_SEC_PROXY_SRC_TARGET_DATA_BASE,
0
}

This structure contains configuration parameters for the sec_proxy IP.