AM243x MCU+ SDK  08.04.00
per_null.h File Reference

Introduction

This file contains the type definitions and helper macros for the "null" peripheral interface.

Go to the source code of this file.

Data Structures

struct  NullPer_Cfg
 Null Peripheral configuration parameters. More...
 
struct  NullPer_Obj
 Null Peripheral object. More...
 

Macros

#define ENET_NULLPER_FEAT1   (ENET_BIT(0U))
 
#define ENET_NULLPER_FEAT2   (ENET_BIT(1U))
 
#define ENET_NULLPER_ERRATA1   (ENET_BIT(0U))
 
#define ENET_NULLPER_CLK_MCLK   (1U)
 

Typedefs

typedef struct NullPer_Obj_s * NullPer_Handle
 Null Periperhal handle. More...
 

Functions

void NullPer_initCfg (EnetPer_Handle hPer, Enet_Type enetType, void *cfg, uint32_t cfgSize)
 Initialize Null peripheral's configuration parameters. More...
 
int32_t NullPer_open (EnetPer_Handle hPer, Enet_Type enetType, uint32_t instId, const void *cfg, uint32_t cfgSize)
 Open and initialize the Null Peripheral. More...
 
int32_t NullPer_rejoin (EnetPer_Handle hPer, Enet_Type enetType, uint32_t instId)
 Rejoin the Null Peripheral. More...
 
int32_t NullPer_ioctl (EnetPer_Handle hPer, uint32_t cmd, Enet_IoctlPrms *prms)
 Issue an operation on the Null Peripheral. More...
 
void NullPer_poll (EnetPer_Handle hPer, uint32_t evtMask)
 Poll for Ethernet events on the Null Peripheral. More...
 
void NullPer_periodicTick (EnetPer_Handle hPer)
 Run periodic tick on the Null Peripheral. More...
 
void NullPer_close (EnetPer_Handle hPer)
 Close the Null Peripheral. More...
 

Macro Definition Documentation

◆ ENET_NULLPER_FEAT1

#define ENET_NULLPER_FEAT1   (ENET_BIT(0U))

Null peripheral dummy feature 1

◆ ENET_NULLPER_FEAT2

#define ENET_NULLPER_FEAT2   (ENET_BIT(1U))

Null peripheral dummy feature 2

◆ ENET_NULLPER_ERRATA1

#define ENET_NULLPER_ERRATA1   (ENET_BIT(0U))

Null peripheral dummy errata 1

◆ ENET_NULLPER_CLK_MCLK

#define ENET_NULLPER_CLK_MCLK   (1U)

Null peripheral MCLK id

Typedef Documentation

◆ NullPer_Handle

typedef struct NullPer_Obj_s* NullPer_Handle

Null Periperhal handle.

Function Documentation

◆ NullPer_initCfg()

void NullPer_initCfg ( EnetPer_Handle  hPer,
Enet_Type  enetType,
void *  cfg,
uint32_t  cfgSize 
)

Initialize Null peripheral's configuration parameters.

Initializes the configuration parameters for a Null periperhal.

Parameters
hPerEnet Peripheral handle
enetTypeEnet Peripheral type
cfgConfiguration parameters to be initialized
cfgSizeSize of the configuration parameters

◆ NullPer_open()

int32_t NullPer_open ( EnetPer_Handle  hPer,
Enet_Type  enetType,
uint32_t  instId,
const void *  cfg,
uint32_t  cfgSize 
)

Open and initialize the Null Peripheral.

Opens and initializes the Null Peripheral with the configuration parameters provided by the caller.

Parameters
hPerEnet Peripheral handle
enetTypeEnet Peripheral type
instIdEnet Peripheral instance id
cfgConfiguration parameters
cfgSizeSize of the configuration parameters
Returns
Enet_ErrorCodes

◆ NullPer_rejoin()

int32_t NullPer_rejoin ( EnetPer_Handle  hPer,
Enet_Type  enetType,
uint32_t  instId 
)

Rejoin the Null Peripheral.

Reopens the Null Peripheral, but doesn't perform any hardware initialization. This function is expected to be called to attach to a running peripheral.

Parameters
hPerEnet Peripheral handle
enetTypeEnet Peripheral type
instIdEnet Peripheral instance id
Returns
Enet_ErrorCodes

◆ NullPer_ioctl()

int32_t NullPer_ioctl ( EnetPer_Handle  hPer,
uint32_t  cmd,
Enet_IoctlPrms prms 
)

Issue an operation on the Null Peripheral.

Issues a control operation on the Null Peripheral.

Parameters
hPerEnet Peripheral handle
cmdIOCTL command Id
prmsIOCTL parameters
Returns
Enet_ErrorCodes

◆ NullPer_poll()

void NullPer_poll ( EnetPer_Handle  hPer,
uint32_t  evtMask 
)

Poll for Ethernet events on the Null Peripheral.

Unblocking poll for the events specified in evtMask.

Parameters
hPerEnet Peripheral handle
evtMaskEvent bit mask

◆ NullPer_periodicTick()

void NullPer_periodicTick ( EnetPer_Handle  hPer)

Run periodic tick on the Null Peripheral.

Run PHY periodic tick on the Ethernet peripheral.

Parameters
hPerEnet Peripheral handle

◆ NullPer_close()

void NullPer_close ( EnetPer_Handle  hPer)

Close the Null Peripheral.

Closes the Null Peripheral.

Parameters
hPerEnet Peripheral handle