AM243x MCU+ SDK  08.04.00

Introduction

This module contains APIs to program and use the PRUICSS module. Programmable Real-Time Unit and Industrial Communication Subsystem(PRUICSS) allows implementation of various high-performance industrial control algorithms and industrial interface standards.

Data Structures

struct  PRUICSS_SysevtToChannelMap
 Data structure used for system event to channel mapping in PRUICSS. More...
 
struct  PRUICSS_ChannelToHostMap
 Data structure used for channel to host map in PRUICSS. More...
 
struct  PRUICSS_IntcInitData
 PRUICSS Interrupt controller initialisation data structure. More...
 
struct  PRUICSS_IrqFunMap
 PRUICSS IRQ handler mapping structure. More...
 
struct  PRUICSS_Object
 PRUICSS Object. More...
 
struct  PRUICSS_HwAttrs
 PRUICSS Hardware Attributes. More...
 
struct  PRUICSS_Config
 PRUICSS Global configuration structure. More...
 

Functions

int32_t PRUICSS_init (void)
 This function initializes the PRUICSS module. More...
 
int32_t PRUICSS_deinit (void)
 This function de-initializes the PRUICSS module. More...
 
PRUICSS_Handle PRUICSS_open (uint32_t instance)
 This function creates the handle for a PRUICSS instance. More...
 
int32_t PRUICSS_close (PRUICSS_Handle handle)
 This function deletes the handle for a PRUICSS instance. More...
 
int32_t PRUICSS_intcInit (PRUICSS_Handle handle, const PRUICSS_IntcInitData *intcInitData)
 This function does Interrupt-Channel-host mapping. More...
 
int32_t PRUICSS_registerIrqHandler (PRUICSS_Handle handle, uint32_t pruEvtoutNum, int32_t intrNum, int32_t eventNum, uint8_t waitEnable, PRUICSS_IrqHandler irqHandler)
 This function registers an Interrupt Handler for an event. More...
 
int32_t PRUICSS_resetCore (PRUICSS_Handle handle, uint8_t pruNum)
 This function resets the PRU. More...
 
int32_t PRUICSS_disableCore (PRUICSS_Handle handle, uint8_t pruNum)
 This function disables the PRU. More...
 
int32_t PRUICSS_enableCore (PRUICSS_Handle handle, uint8_t pruNum)
 This function enables the PRU. More...
 
uint32_t PRUICSS_initMemory (PRUICSS_Handle handle, uint32_t pruicssMem)
 This function initializes the PRU memory to zero. More...
 
uint32_t PRUICSS_writeMemory (PRUICSS_Handle handle, uint32_t pruicssMem, uint32_t wordoffset, const uint32_t *source_mem, uint32_t bytelength)
 This function writes the given data to PRU memory. More...
 
uint32_t PRUICSS_readMemory (PRUICSS_Handle handle, uint32_t pruicssMem, uint32_t wordoffset, uint32_t *dest_mem, uint32_t bytelength)
 This function reads from PRU memory and stores in block of memory. More...
 
int32_t PRUICSS_sendEvent (PRUICSS_Handle handle, uint32_t eventnum)
 This function generates an INTC event. It should be called only after successful execution of PRUICSS_intcInit(). More...
 
int32_t PRUICSS_waitEvent (PRUICSS_Handle handle, uint32_t pruEvtoutNum)
 This function waits for a system event to happen. It should be called only after successful execution of PRUICSS_intcInit(). More...
 
int32_t PRUICSS_clearEvent (PRUICSS_Handle handle, uint32_t eventnum)
 This function clears an INTC event. It should be called only after successful execution of PRUICSS_intcInit(). More...
 
int32_t PRUICSS_sendWaitClearEvent (PRUICSS_Handle handle, uint32_t sendEventNum, uint32_t pruEvtoutNum, uint32_t ackEventNum)
 This function generates an INTC event, waits for AINTC event and clears an INTC event. More...
 
uint32_t PRUICSS_getVersion (PRUICSS_Handle handle)
 Get PRUICSS version number from ICSSCFG_REVID register. More...
 
int32_t PRUICSS_setConstantTblEntry (PRUICSS_Handle handle, uint8_t pruNum, int32_t constantTblEntry, uint32_t constantTblVal)
 This API updates the constant table for specified constant table entry which have write permissions. More...
 
int32_t PRUICSS_setIepClkSrc (PRUICSS_Handle handle, uint32_t source)
 This API configures the source of the IEP clock to be either IEP CLK as the source or ICSSGn_CORE_CLK. More...
 
int32_t PRUICSS_setGpMuxSelect (PRUICSS_Handle handle, uint8_t pruNum, uint8_t mode)
 This API sets the GP Mux Select mode for a specific PRU. More...
 
int32_t PRUICSS_setGpiMode (PRUICSS_Handle handle, uint8_t pruNum, uint8_t mode)
 This API sets the GPI mode for a specific PRU. More...
 
int32_t PRUICSS_setSaMuxMode (PRUICSS_Handle handle, uint8_t mode)
 This API sets the G_MUX_EN mux field in ICSSG_SA_MX_REG register. More...
 
int32_t PRUICSS_configureCycleCounter (PRUICSS_Handle handle, uint8_t pruNum, uint8_t enable)
 This function enables/disables the PRU Cycle Counter for a core. More...
 
int32_t PRUICSS_controlIepCounter (PRUICSS_Handle handle, uint8_t iepInstance, uint8_t enable)
 This API enables/disables the counter in IEP module. More...
 
int32_t PRUICSS_setIepCounterIncrementValue (PRUICSS_Handle handle, uint8_t iepInstance, uint8_t value)
 This API sets the default increment value for counter in IEP module. This value is used when compensation is not active. More...
 
int32_t PRUICSS_readEfuse (PRUICSS_Handle handle, uint8_t *data)
 This API reads the state of efuse bits from ICSSG_HWDIS_REG register. More...
 
int32_t PRUICSS_setIcssCfgMiiMode (PRUICSS_Handle handle, uint8_t miiInstance, uint8_t mode)
 This API sets the MII mode in MII_G_RT_ICSS_G_CFG register. More...
 
int32_t PRUICSS_setIcssCfgTxFifo (PRUICSS_Handle handle, uint8_t fifoInstance, uint8_t enable)
 This API configures the TX FIFO to be used. More...
 
const PRUICSS_HwAttrsPRUICSS_getAttrs (uint32_t instance)
 Return PRUICSS attributes. More...
 

Typedefs

typedef void(* PRUICSS_IrqHandler) (void *buf)
 
typedef struct PRUICSS_Config_s * PRUICSS_Handle
 A handle that is returned from a PRUICSS_open() call. This handle is required for calling other APIs. More...
 

Macros

#define PRUICSS_NUM_CORES   (6U)
 Number of different cores present in PRUICSS. More...
 
#define PRUICSS_INTC_NUM_HOST_INTERRUPTS   (20U)
 Number of Host Interrupts supported in PRUICSS Local INTC. More...
 
#define PRUICSS_INTC_NUM_CHANNELS   (20U)
 Number of Output Interrupt channels supported in PRUICSS Local INTC. More...
 
#define PRUICSS_INTC_NUM_SYS_EVTS   (160U)
 Number of Events that can be captured in PRUICSS Local INTC. More...
 
#define PRUICSS_NUM_GP_MUX_SEL_MODES   (4U)
 Number of different GP MUX Selections modes. More...
 
#define PRUICSS_NUM_GPI_MODES   (4U)
 Number of different GPI modes. More...
 
#define PRUICSS_NUM_SA_MUX_MODES   (2U)
 Number of different PRUICSS SA MUX Modes. More...
 
#define PRUICSS_NUM_ICSS_CFG_MII_MODES   (3U)
 Number of different ICSS_G_CFG MII Modes. More...
 

PRUICSS Cores

Different cores present in PRUICSS

#define PRUICSS_PRU0   (0U)
 
#define PRUICSS_PRU1   (1U)
 
#define PRUICSS_RTU_PRU0   (2U)
 
#define PRUICSS_RTU_PRU1   (3U)
 
#define PRUICSS_TX_PRU0   (4U)
 
#define PRUICSS_TX_PRU1   (5U)
 

PRUICSS Memory Offsets

Offsets for different memory inside each PRUICSS instance.

#define PRUICSS_DATARAM(n)   (0x00000U + ((n) * 0x02000U))
 Data RAM0/RAM1. n = 0 for RAM0, n = 1 for RAM1. More...
 
#define PRUICSS_IRAM_RTU_PRU(n)   (0x04000U + ((n) * 0x02000U))
 IRAM for RTU_PRU0/RTU_PRU1. n = 0 for RTU_PRU0,n = 1 for RTU_PRU1. More...
 
#define PRUICSS_IRAM_TX_PRU(n)   (0x0A000U + ((n) * 0x02000U))
 IRAM for TX_PRU0/TX_PRU1. n = 0 for TX_PRU0,n = 1 for TX_PRU1. More...
 
#define PRUICSS_SHARED_RAM   (0x10000U)
 Data RAM2 (shared) More...
 
#define PRUICSS_IRAM_PRU(n)   (0x34000U + ((n) * 0x04000U))
 IRAM for PRU0/PRU1. n = 0 for PRU0,n = 1 for PRU1. More...
 

Index for PRU Constant Table Entries

Index to be used while making calls to PRUICSS_setConstantTblEntry()

#define PRUICSS_CONST_TBL_ENTRY_C24   (0U)
 
#define PRUICSS_CONST_TBL_ENTRY_C25   (1U)
 
#define PRUICSS_CONST_TBL_ENTRY_C26   (2U)
 
#define PRUICSS_CONST_TBL_ENTRY_C27   (3U)
 
#define PRUICSS_CONST_TBL_ENTRY_C28   (4U)
 
#define PRUICSS_CONST_TBL_ENTRY_C29   (5U)
 
#define PRUICSS_CONST_TBL_ENTRY_C30   (6U)
 
#define PRUICSS_CONST_TBL_ENTRY_C31   (7U)
 
#define PRUICSS_NUM_CONST_TBL_ENTRY   (8U)
 

GP MUX Select Modes

#define PRUICSS_GP_MUX_SEL_MODE_GP   (0U)
 
#define PRUICSS_GP_MUX_SEL_MODE_ENDAT   (1U)
 
#define PRUICSS_GP_MUX_SEL_MODE_MII   (2U)
 
#define PRUICSS_GP_MUX_SEL_MODE_SD   (3U)
 

GPI Modes

#define PRUICSS_GPI_MODE_DIRECT_R31_STATUS   (0U)
 Direct connect of PRU[0/1]_r31_status[29:0]. More...
 
#define PRUICSS_GPI_MODE_PARALLEL_16_BIT_CAPTURE   (1U)
 Parallel 16-bit capture mode. PRU[0/1]_r31_status [15:0] is captured using PRU[0/1]_r31_status [16]. More...
 
#define PRUICSS_GPI_MODE_29_BIT_SHIFT   (2U)
 29-bit shift. PRU[0/1]_r31_status[0] -> r31_status[0] -> r31_status[1] -> r_status[28] -> bit bucket More...
 
#define PRUICSS_GPI_MODE_MII_RT   (3U)
 mii_rt mode. Selects mii_rt PRU[0/1] bus More...
 

PRUICSS SA MUX Modes

#define PRUICSS_SA_MUX_MODE_DEFAULT   (0U)
 Default/Legacy Mode. More...
 
#define PRUICSS_SA_MUX_MODE_SD_ENDAT   (1U)
 Few SD and EnDAT pins get remapped to enable different usecase. More...
 

ICSS_G_CFG MII Modes

#define PRUICSS_ICSS_CFG_MII_MODE_MII   (0U)
 MII Mode. More...
 
#define PRUICSS_ICSS_CFG_MII_MODE_RGMII   (1U)
 RGMII Mode. More...
 
#define PRUICSS_ICSS_CFG_MII_MODE_SGMII   (2U)
 SGMII mode. It is supported only for PRU_ICSSG instance. More...
 

PRUICSS TX FIFO Modes

#define PRUICSS_TX_L1_FIFO   (0U)
 
#define PRUICSS_TX_L2_FIFO   (1U)
 

Macro Definition Documentation

◆ PRUICSS_PRU0

#define PRUICSS_PRU0   (0U)

◆ PRUICSS_PRU1

#define PRUICSS_PRU1   (1U)

◆ PRUICSS_RTU_PRU0

#define PRUICSS_RTU_PRU0   (2U)

◆ PRUICSS_RTU_PRU1

#define PRUICSS_RTU_PRU1   (3U)

◆ PRUICSS_TX_PRU0

#define PRUICSS_TX_PRU0   (4U)

◆ PRUICSS_TX_PRU1

#define PRUICSS_TX_PRU1   (5U)

◆ PRUICSS_NUM_CORES

#define PRUICSS_NUM_CORES   (6U)

Number of different cores present in PRUICSS.

◆ PRUICSS_DATARAM

#define PRUICSS_DATARAM (   n)    (0x00000U + ((n) * 0x02000U))

Data RAM0/RAM1. n = 0 for RAM0, n = 1 for RAM1.

◆ PRUICSS_IRAM_RTU_PRU

#define PRUICSS_IRAM_RTU_PRU (   n)    (0x04000U + ((n) * 0x02000U))

IRAM for RTU_PRU0/RTU_PRU1. n = 0 for RTU_PRU0,n = 1 for RTU_PRU1.

◆ PRUICSS_IRAM_TX_PRU

#define PRUICSS_IRAM_TX_PRU (   n)    (0x0A000U + ((n) * 0x02000U))

IRAM for TX_PRU0/TX_PRU1. n = 0 for TX_PRU0,n = 1 for TX_PRU1.

◆ PRUICSS_SHARED_RAM

#define PRUICSS_SHARED_RAM   (0x10000U)

Data RAM2 (shared)

◆ PRUICSS_IRAM_PRU

#define PRUICSS_IRAM_PRU (   n)    (0x34000U + ((n) * 0x04000U))

IRAM for PRU0/PRU1. n = 0 for PRU0,n = 1 for PRU1.

◆ PRUICSS_INTC_NUM_HOST_INTERRUPTS

#define PRUICSS_INTC_NUM_HOST_INTERRUPTS   (20U)

Number of Host Interrupts supported in PRUICSS Local INTC.

◆ PRUICSS_INTC_NUM_CHANNELS

#define PRUICSS_INTC_NUM_CHANNELS   (20U)

Number of Output Interrupt channels supported in PRUICSS Local INTC.

◆ PRUICSS_INTC_NUM_SYS_EVTS

#define PRUICSS_INTC_NUM_SYS_EVTS   (160U)

Number of Events that can be captured in PRUICSS Local INTC.

◆ PRUICSS_CONST_TBL_ENTRY_C24

#define PRUICSS_CONST_TBL_ENTRY_C24   (0U)

◆ PRUICSS_CONST_TBL_ENTRY_C25

#define PRUICSS_CONST_TBL_ENTRY_C25   (1U)

◆ PRUICSS_CONST_TBL_ENTRY_C26

#define PRUICSS_CONST_TBL_ENTRY_C26   (2U)

◆ PRUICSS_CONST_TBL_ENTRY_C27

#define PRUICSS_CONST_TBL_ENTRY_C27   (3U)

◆ PRUICSS_CONST_TBL_ENTRY_C28

#define PRUICSS_CONST_TBL_ENTRY_C28   (4U)

◆ PRUICSS_CONST_TBL_ENTRY_C29

#define PRUICSS_CONST_TBL_ENTRY_C29   (5U)

◆ PRUICSS_CONST_TBL_ENTRY_C30

#define PRUICSS_CONST_TBL_ENTRY_C30   (6U)

◆ PRUICSS_CONST_TBL_ENTRY_C31

#define PRUICSS_CONST_TBL_ENTRY_C31   (7U)

◆ PRUICSS_NUM_CONST_TBL_ENTRY

#define PRUICSS_NUM_CONST_TBL_ENTRY   (8U)

◆ PRUICSS_GP_MUX_SEL_MODE_GP

#define PRUICSS_GP_MUX_SEL_MODE_GP   (0U)

◆ PRUICSS_GP_MUX_SEL_MODE_ENDAT

#define PRUICSS_GP_MUX_SEL_MODE_ENDAT   (1U)

◆ PRUICSS_GP_MUX_SEL_MODE_MII

#define PRUICSS_GP_MUX_SEL_MODE_MII   (2U)

◆ PRUICSS_GP_MUX_SEL_MODE_SD

#define PRUICSS_GP_MUX_SEL_MODE_SD   (3U)

◆ PRUICSS_NUM_GP_MUX_SEL_MODES

#define PRUICSS_NUM_GP_MUX_SEL_MODES   (4U)

Number of different GP MUX Selections modes.

◆ PRUICSS_GPI_MODE_DIRECT_R31_STATUS

#define PRUICSS_GPI_MODE_DIRECT_R31_STATUS   (0U)

Direct connect of PRU[0/1]_r31_status[29:0].

◆ PRUICSS_GPI_MODE_PARALLEL_16_BIT_CAPTURE

#define PRUICSS_GPI_MODE_PARALLEL_16_BIT_CAPTURE   (1U)

Parallel 16-bit capture mode. PRU[0/1]_r31_status [15:0] is captured using PRU[0/1]_r31_status [16].

◆ PRUICSS_GPI_MODE_29_BIT_SHIFT

#define PRUICSS_GPI_MODE_29_BIT_SHIFT   (2U)

29-bit shift. PRU[0/1]_r31_status[0] -> r31_status[0] -> r31_status[1] -> r_status[28] -> bit bucket

◆ PRUICSS_GPI_MODE_MII_RT

#define PRUICSS_GPI_MODE_MII_RT   (3U)

mii_rt mode. Selects mii_rt PRU[0/1] bus

◆ PRUICSS_NUM_GPI_MODES

#define PRUICSS_NUM_GPI_MODES   (4U)

Number of different GPI modes.

◆ PRUICSS_SA_MUX_MODE_DEFAULT

#define PRUICSS_SA_MUX_MODE_DEFAULT   (0U)

Default/Legacy Mode.

◆ PRUICSS_SA_MUX_MODE_SD_ENDAT

#define PRUICSS_SA_MUX_MODE_SD_ENDAT   (1U)

Few SD and EnDAT pins get remapped to enable different usecase.

◆ PRUICSS_NUM_SA_MUX_MODES

#define PRUICSS_NUM_SA_MUX_MODES   (2U)

Number of different PRUICSS SA MUX Modes.

◆ PRUICSS_ICSS_CFG_MII_MODE_MII

#define PRUICSS_ICSS_CFG_MII_MODE_MII   (0U)

MII Mode.

◆ PRUICSS_ICSS_CFG_MII_MODE_RGMII

#define PRUICSS_ICSS_CFG_MII_MODE_RGMII   (1U)

RGMII Mode.

◆ PRUICSS_ICSS_CFG_MII_MODE_SGMII

#define PRUICSS_ICSS_CFG_MII_MODE_SGMII   (2U)

SGMII mode. It is supported only for PRU_ICSSG instance.

◆ PRUICSS_NUM_ICSS_CFG_MII_MODES

#define PRUICSS_NUM_ICSS_CFG_MII_MODES   (3U)

Number of different ICSS_G_CFG MII Modes.

◆ PRUICSS_TX_L1_FIFO

#define PRUICSS_TX_L1_FIFO   (0U)

◆ PRUICSS_TX_L2_FIFO

#define PRUICSS_TX_L2_FIFO   (1U)

Typedef Documentation

◆ PRUICSS_IrqHandler

typedef void(* PRUICSS_IrqHandler) (void *buf)

◆ PRUICSS_Handle

typedef struct PRUICSS_Config_s* PRUICSS_Handle

A handle that is returned from a PRUICSS_open() call. This handle is required for calling other APIs.

Function Documentation

◆ PRUICSS_init()

int32_t PRUICSS_init ( void  )

This function initializes the PRUICSS module.

Returns
SystemP_SUCCESS in case of success, SystemP_FAILURE otherwise

◆ PRUICSS_deinit()

int32_t PRUICSS_deinit ( void  )

This function de-initializes the PRUICSS module.

Returns
SystemP_SUCCESS in case of success, SystemP_FAILURE otherwise

◆ PRUICSS_open()

PRUICSS_Handle PRUICSS_open ( uint32_t  instance)

This function creates the handle for a PRUICSS instance.

Parameters
instancePRUICSS instance number
Returns
A PRUICSS_Handle on success or a NULL on an error

◆ PRUICSS_close()

int32_t PRUICSS_close ( PRUICSS_Handle  handle)

This function deletes the handle for a PRUICSS instance.

Parameters
handlePRUICSS_Handle returned from PRUICSS_open()
Returns
SystemP_SUCCESS in case of success, SystemP_FAILURE otherwise

◆ PRUICSS_intcInit()

int32_t PRUICSS_intcInit ( PRUICSS_Handle  handle,
const PRUICSS_IntcInitData intcInitData 
)

This function does Interrupt-Channel-host mapping.

Parameters
handlePRUICSS_Handle returned from PRUICSS_open()
intcInitDataPointer to structure of type PRUICSS_IntcInitData containing mapping information
Returns
SystemP_SUCCESS in case of success, SystemP_FAILURE otherwise

◆ PRUICSS_registerIrqHandler()

int32_t PRUICSS_registerIrqHandler ( PRUICSS_Handle  handle,
uint32_t  pruEvtoutNum,
int32_t  intrNum,
int32_t  eventNum,
uint8_t  waitEnable,
PRUICSS_IrqHandler  irqHandler 
)

This function registers an Interrupt Handler for an event.

Parameters
handlePRUICSS_Handle returned from PRUICSS_open()
pruEvtoutNumThe ARM side event number
intrNumInterrupt number of R5F
eventNumEvent number of PRUICSS
waitEnableFlag specifying whether application can wait on this interrupt using PRUICSS_waitEvent() function. 1 for enable, 0 for disable
irqHandlerPointer to a function which will be called on interrupt
Returns
SystemP_SUCCESS in case of successful registration, SystemP_FAILURE otherwise

◆ PRUICSS_resetCore()

int32_t PRUICSS_resetCore ( PRUICSS_Handle  handle,
uint8_t  pruNum 
)

This function resets the PRU.

Parameters
handlePRUICSS_Handle returned from PRUICSS_open()
pruNumPRU core number from PRUICSS_Cores
Returns
SystemP_SUCCESS in case of successful reset, SystemP_FAILURE otherwise

◆ PRUICSS_disableCore()

int32_t PRUICSS_disableCore ( PRUICSS_Handle  handle,
uint8_t  pruNum 
)

This function disables the PRU.

Parameters
handlePRUICSS_Handle returned from PRUICSS_open()
pruNumPRU core number from PRUICSS_Cores
Returns
SystemP_SUCCESS in case of successful disable, SystemP_FAILURE otherwise

◆ PRUICSS_enableCore()

int32_t PRUICSS_enableCore ( PRUICSS_Handle  handle,
uint8_t  pruNum 
)

This function enables the PRU.

Parameters
handlePRUICSS_Handle returned from PRUICSS_open()
pruNumPRU core number from PRUICSS_Cores
Returns
SystemP_SUCCESS in case of successful enable, SystemP_FAILURE otherwise

◆ PRUICSS_initMemory()

uint32_t PRUICSS_initMemory ( PRUICSS_Handle  handle,
uint32_t  pruicssMem 
)

This function initializes the PRU memory to zero.

Parameters
handlePRUICSS_Handle returned from PRUICSS_open()
pruicssMemPRUICSS Memory macro from PRUICSS_MemoryOffsets
Returns
Word length written or 0 on error

◆ PRUICSS_writeMemory()

uint32_t PRUICSS_writeMemory ( PRUICSS_Handle  handle,
uint32_t  pruicssMem,
uint32_t  wordoffset,
const uint32_t *  source_mem,
uint32_t  bytelength 
)

This function writes the given data to PRU memory.

Parameters
handlePRUICSS_Handle returned from PRUICSS_open()
pruicssMemPRUICSS Memory macro from PRUICSS_MemoryOffsets
wordoffsetOffset at which the write will happen
source_memSource memory[ Array of uint32_t integers ]
bytelengthTotal number of bytes to be writen
Returns
Word length written or 0 on error

◆ PRUICSS_readMemory()

uint32_t PRUICSS_readMemory ( PRUICSS_Handle  handle,
uint32_t  pruicssMem,
uint32_t  wordoffset,
uint32_t *  dest_mem,
uint32_t  bytelength 
)

This function reads from PRU memory and stores in block of memory.

Parameters
handlePRUICSS_Handle returned from PRUICSS_open()
pruicssMemPRUICSS Memory macro from PRUICSS_MemoryOffsets
wordoffsetOffset at which the read will happen
dest_memDestination memory[ Array of uint32_t integers ]
bytelengthTotal number of bytes to be read
Returns
Word length read or 0 on error

◆ PRUICSS_sendEvent()

int32_t PRUICSS_sendEvent ( PRUICSS_Handle  handle,
uint32_t  eventnum 
)

This function generates an INTC event. It should be called only after successful execution of PRUICSS_intcInit().

Parameters
handlePRUICSS_Handle returned from PRUICSS_open()
eventnumThe INTC Event number
Returns
SystemP_SUCCESS in case of successful transition, SystemP_FAILURE otherwise

◆ PRUICSS_waitEvent()

int32_t PRUICSS_waitEvent ( PRUICSS_Handle  handle,
uint32_t  pruEvtoutNum 
)

This function waits for a system event to happen. It should be called only after successful execution of PRUICSS_intcInit().

Parameters
handlePRUICSS_Handle returned from PRUICSS_open()
pruEvtoutNumThe AINTC Event number
Returns
SystemP_SUCCESS in case of successful transition, SystemP_FAILURE otherwise

◆ PRUICSS_clearEvent()

int32_t PRUICSS_clearEvent ( PRUICSS_Handle  handle,
uint32_t  eventnum 
)

This function clears an INTC event. It should be called only after successful execution of PRUICSS_intcInit().

Parameters
handlePRUICSS_Handle returned from PRUICSS_open()
eventnumThe INTC Event number
Returns
SystemP_SUCCESS in case of successful transition, SystemP_FAILURE otherwise

◆ PRUICSS_sendWaitClearEvent()

int32_t PRUICSS_sendWaitClearEvent ( PRUICSS_Handle  handle,
uint32_t  sendEventNum,
uint32_t  pruEvtoutNum,
uint32_t  ackEventNum 
)

This function generates an INTC event, waits for AINTC event and clears an INTC event.

Parameters
handlePRUICSS_Handle returned from PRUICSS_open()
sendEventNumEvent number
pruEvtoutNumPRU Event number
ackEventNumAcknowledgement event number
Returns
SystemP_SUCCESS in case of successful transition, SystemP_FAILURE otherwise

◆ PRUICSS_getVersion()

uint32_t PRUICSS_getVersion ( PRUICSS_Handle  handle)

Get PRUICSS version number from ICSSCFG_REVID register.

Parameters
handlePRUICSS_Handle returned from PRUICSS_open()
Returns
PRU ICSS version

◆ PRUICSS_setConstantTblEntry()

int32_t PRUICSS_setConstantTblEntry ( PRUICSS_Handle  handle,
uint8_t  pruNum,
int32_t  constantTblEntry,
uint32_t  constantTblVal 
)

This API updates the constant table for specified constant table entry which have write permissions.

Parameters
handlePRUICSS_Handle returned from PRUICSS_open()
pruNumPRU number[0 or 1] for which constant table is being updated
constantTblEntrycontant table entry being updated
constantTblValcontant table value to be written
Returns
SystemP_SUCCESS on success, SystemP_FAILURE on error

◆ PRUICSS_setIepClkSrc()

int32_t PRUICSS_setIepClkSrc ( PRUICSS_Handle  handle,
uint32_t  source 
)

This API configures the source of the IEP clock to be either IEP CLK as the source or ICSSGn_CORE_CLK.

Parameters
handlePRUICSS_Handle returned from PRUICSS_open()
sourcesource of the IEP clock (0 for IEP CLK, 1 for ICSSGn_CORE_CLK)
Returns
SystemP_SUCCESS on success, SystemP_FAILURE on error

◆ PRUICSS_setGpMuxSelect()

int32_t PRUICSS_setGpMuxSelect ( PRUICSS_Handle  handle,
uint8_t  pruNum,
uint8_t  mode 
)

This API sets the GP Mux Select mode for a specific PRU.

Parameters
handlePRUICSS_Handle returned from PRUICSS_open()
pruNumPRUICSS_PRU0 or PRUICSS_PRU1
modeMode from PRUICSS_GpMuxSelectModes
Returns
SystemP_SUCCESS on success, SystemP_FAILURE on error

◆ PRUICSS_setGpiMode()

int32_t PRUICSS_setGpiMode ( PRUICSS_Handle  handle,
uint8_t  pruNum,
uint8_t  mode 
)

This API sets the GPI mode for a specific PRU.

Parameters
handlePRUICSS_Handle returned from PRUICSS_open()
pruNumPRUICSS_PRU0 or PRUICSS_PRU1
modeMode from PRUICSS_GpiModes
Returns
SystemP_SUCCESS on success, SystemP_FAILURE on error

◆ PRUICSS_setSaMuxMode()

int32_t PRUICSS_setSaMuxMode ( PRUICSS_Handle  handle,
uint8_t  mode 
)

This API sets the G_MUX_EN mux field in ICSSG_SA_MX_REG register.

Parameters
handlePRUICSS_Handle returned from PRUICSS_open()
modeMode from PRUICSS_SaMuxModes
Returns
SystemP_SUCCESS on success, SystemP_FAILURE on error

◆ PRUICSS_configureCycleCounter()

int32_t PRUICSS_configureCycleCounter ( PRUICSS_Handle  handle,
uint8_t  pruNum,
uint8_t  enable 
)

This function enables/disables the PRU Cycle Counter for a core.

Parameters
handlePRUICSS_Handle returned from PRUICSS_open()
pruNumPRU core number from PRUICSS_Cores
enable0 for disable, 1 for enable
Returns
SystemP_SUCCESS in case of successful enable, SystemP_FAILURE otherwise

◆ PRUICSS_controlIepCounter()

int32_t PRUICSS_controlIepCounter ( PRUICSS_Handle  handle,
uint8_t  iepInstance,
uint8_t  enable 
)

This API enables/disables the counter in IEP module.

Parameters
handlePRUICSS_Handle returned from PRUICSS_open()
iepInstance0 for IEP0, 1 for IEP1
enable0 for disabling the counter, 1 for enabling the counter
Returns
SystemP_SUCCESS on success, SystemP_FAILURE on error

◆ PRUICSS_setIepCounterIncrementValue()

int32_t PRUICSS_setIepCounterIncrementValue ( PRUICSS_Handle  handle,
uint8_t  iepInstance,
uint8_t  value 
)

This API sets the default increment value for counter in IEP module. This value is used when compensation is not active.

Parameters
handlePRUICSS_Handle returned from PRUICSS_open()
iepInstance0 for IEP0, 1 for IEP1
valueIncrement value. Maximum value allowed is 15
Returns
SystemP_SUCCESS on success, SystemP_FAILURE on error

◆ PRUICSS_readEfuse()

int32_t PRUICSS_readEfuse ( PRUICSS_Handle  handle,
uint8_t *  data 
)

This API reads the state of efuse bits from ICSSG_HWDIS_REG register.

Parameters
handlePRUICSS_Handle returned from PRUICSS_open()
datadata read from the register
Returns
SystemP_SUCCESS on success, SystemP_FAILURE on error

◆ PRUICSS_setIcssCfgMiiMode()

int32_t PRUICSS_setIcssCfgMiiMode ( PRUICSS_Handle  handle,
uint8_t  miiInstance,
uint8_t  mode 
)

This API sets the MII mode in MII_G_RT_ICSS_G_CFG register.

Parameters
handlePRUICSS_Handle returned from PRUICSS_open()
miiInstance0 for MII0_MODE, 1 for MII1_MODE
modeMode from PRUICSS_IcssCfgMiiModes
Returns
SystemP_SUCCESS on success, SystemP_FAILURE on error

◆ PRUICSS_setIcssCfgTxFifo()

int32_t PRUICSS_setIcssCfgTxFifo ( PRUICSS_Handle  handle,
uint8_t  fifoInstance,
uint8_t  enable 
)

This API configures the TX FIFO to be used.

Parameters
handlePRUICSS_Handle returned from PRUICSS_open()
fifoInstanceFIFO from PRUICSS_TxFifos
enable0 for disable, 1 for enable
Returns
SystemP_SUCCESS on success, SystemP_FAILURE on error

◆ PRUICSS_getAttrs()

const PRUICSS_HwAttrs* PRUICSS_getAttrs ( uint32_t  instance)

Return PRUICSS attributes.

Parameters
instancePRUICSS instance
Returns
PRUICSS_HwAttrs, else NULL if instance is invalid