AM243x MCU+ SDK  08.04.00
enetphy.h File Reference

Introduction

This file contains the type definitions and helper macros for the Ethernet PHY interface.

Go to the source code of this file.

Data Structures

struct  EnetPhy_Version
 PHY version (ID). More...
 
struct  EnetPhy_LinkCfg
 Link speed and duplexity configuration. More...
 
struct  EnetPhy_FsmTimeoutCfg
 PHY State-Machine time-out values. More...
 
struct  EnetPhy_Cfg
 PHY configuration parameters. More...
 
struct  EnetPhy_Mdio
 MDIO driver. More...
 
struct  EnetPhy_State
 PHY driver FSM state. More...
 
struct  EnetPhy_Obj
 PHY driver object. More...
 

Macros

#define ENETPHY_IS_ADDR_VALID(addr)   ((addr) <= 31U)
 Check if PHY address is valid (0 - 31). More...
 
#define ENETPHY_BIT(n)   (1U << (n))
 Macro to set bit at given bit position. More...
 
#define ENETPHY_IS_BIT_SET(val, n)   (((val) & ENETPHY_BIT(n)) != 0U)
 Macro to check if bit at given bit position is set. More...
 
#define ENETPHY_ARRAYSIZE(x)   (sizeof(x) / sizeof(x[0]))
 Macro to get the size of an array. More...
 
#define ENETPHY_EXTENDED_CFG_SIZE_MAX   (128U)
 Max extended configuration size, arbitrarily chosen. More...
 
#define ENETPHY_FSM_TICK_PERIOD_MS   (100U)
 Enet PHY State Machine tick period. More...
 
#define ENETPHY_INVALID_PHYADDR   (~0U)
 Invalid PHY address indicator. More...
 
Ethernet PHY driver error codes

Error codes returned by the Ethernet PHY driver APIs.

#define ENETPHY_SOK   (CSL_PASS)
 Success. More...
 
#define ENETPHY_EFAIL   (CSL_EFAIL)
 Generic failure error condition (typically caused by hardware). More...
 
#define ENETPHY_EBADARGS   (CSL_EBADARGS)
 Bad arguments (i.e. NULL pointer). More...
 
#define ENETPHY_EINVALIDPARAMS   (CSL_EINVALID_PARAMS)
 Invalid parameters (i.e. value out-of-range). More...
 
#define ENETPHY_ETIMEOUT   (CSL_ETIMEOUT)
 Time out while waiting for a given condition to happen. More...
 
#define ENETPHY_EALLOC   (CSL_EALLOC)
 Allocation failure. More...
 
#define ENETPHY_EPERM   (CSL_EALLOC - 4)
 Operation not permitted. More...
 
#define ENETPHY_ENOTSUPPORTED   (CSL_EALLOC - 5)
 Operation not supported. More...
 
Ethernet PHY link capability masks

Error codes returned by the Ethernet PHY driver APIs.

#define ENETPHY_LINK_CAP_HD10   ENETPHY_BIT(1)
 10-Mbps, half-duplex capability mask. More...
 
#define ENETPHY_LINK_CAP_FD10   ENETPHY_BIT(2)
 10-Mbps, full-duplex capability mask. More...
 
#define ENETPHY_LINK_CAP_HD100   ENETPHY_BIT(3)
 100-Mbps, half-duplex capability mask. More...
 
#define ENETPHY_LINK_CAP_FD100   ENETPHY_BIT(4)
 100-Mbps, full-duplex capability mask. More...
 
#define ENETPHY_LINK_CAP_HD1000   ENETPHY_BIT(5)
 1-Gbps, half-duplex capability mask. More...
 
#define ENETPHY_LINK_CAP_FD1000   ENETPHY_BIT(6)
 1-Gbps, full-duplex capability mask. More...
 
#define ENETPHY_LINK_CAP_10
 10-Mbps, full and half-duplex capability mask. More...
 
#define ENETPHY_LINK_CAP_100
 100-Mbps, full and half-duplex capability mask. More...
 
#define ENETPHY_LINK_CAP_1000
 1-Gbps, full and half-duplex capability mask. More...
 
#define ENETPHY_LINK_CAP_ALL
 Auto-negotiation mask with all duplexity and speed values set. More...
 

Typedefs

typedef EnetPhy_MdioEnetPhy_MdioHandle
 MDIO driver handle. More...
 
typedef struct EnetPhy_Drv_s * EnetPhyDrv_Handle
 PHY specific driver handle. More...
 
typedef struct EnetPhy_Obj_s * EnetPhy_Handle
 PHY driver object handle. More...
 

Enumerations

enum  EnetPhy_Magic { ENETPHY_MAGIC = 0xCADACADAU, ENETPHY_NO_MAGIC = 0x0U }
 EnetPhy driver magic value, used to indicate if driver is open or not. More...
 
enum  EnetPhy_Mii {
  ENETPHY_MAC_MII_MII = 0U, ENETPHY_MAC_MII_RMII, ENETPHY_MAC_MII_GMII, ENETPHY_MAC_MII_RGMII,
  ENETPHY_MAC_MII_SGMII, ENETPHY_MAC_MII_QSGMII
}
 MAC Media-Independent Interface (MII). More...
 
enum  EnetPhy_Speed { ENETPHY_SPEED_10MBIT = 0U, ENETPHY_SPEED_100MBIT, ENETPHY_SPEED_1GBIT, ENETPHY_SPEED_AUTO }
 MAC interface speed. More...
 
enum  EnetPhy_Duplexity { ENETPHY_DUPLEX_HALF = 0U, ENETPHY_DUPLEX_FULL, ENETPHY_DUPLEX_AUTO }
 MAC interface duplexity. More...
 
enum  EnetPhy_LinkStatus { ENETPHY_GOT_LINK = 0U, ENETPHY_LINK_UP, ENETPHY_LOST_LINK, ENETPHY_LINK_DOWN }
 PHY link status. More...
 
enum  EnetPhy_FsmState {
  ENETPHY_FSM_STATE_INIT = 0U, ENETPHY_FSM_STATE_FINDING, ENETPHY_FSM_STATE_RESET_WAIT, ENETPHY_FSM_STATE_ENABLE,
  ENETPHY_FSM_STATE_FOUND, ENETPHY_FSM_STATE_NWAY_START, ENETPHY_FSM_STATE_NWAY_WAIT, ENETPHY_FSM_STATE_LINK_WAIT,
  ENETPHY_FSM_STATE_LINKED, ENETPHY_FSM_STATE_LOOPBACK
}
 PHY driver state-machine states. More...
 

Functions

void EnetPhy_initCfg (EnetPhy_Cfg *phyCfg)
 Initialize PHY config params. More...
 
void EnetPhy_setExtendedCfg (EnetPhy_Cfg *phyCfg, const void *extendedCfg, uint32_t extendedCfgSize)
 Set PHY extended parameters. More...
 
EnetPhy_Handle EnetPhy_open (const EnetPhy_Cfg *phyCfg, EnetPhy_Mii mii, const EnetPhy_LinkCfg *linkCfg, uint32_t macPortCaps, EnetPhy_MdioHandle hMdio, void *mdioArgs)
 Open the PHY driver. More...
 
void EnetPhy_close (EnetPhy_Handle hPhy)
 Close the PHY driver. More...
 
EnetPhy_LinkStatus EnetPhy_tick (EnetPhy_Handle hPhy)
 Run PHY state machine. More...
 
int32_t EnetPhy_getId (EnetPhy_Handle hPhy, EnetPhy_Version *version)
 Get PHY id. More...
 
bool EnetPhy_isAlive (EnetPhy_Handle hPhy)
 Get PHY alive status. More...
 
bool EnetPhy_isLinked (EnetPhy_Handle hPhy)
 Get link status. More...
 
int32_t EnetPhy_getLinkCfg (EnetPhy_Handle hPhy, EnetPhy_LinkCfg *linkCfg)
 Get link configuration. More...
 
int32_t EnetPhy_readReg (EnetPhy_Handle hPhy, uint32_t reg, uint16_t *val)
 Read PHY register. More...
 
int32_t EnetPhy_writeReg (EnetPhy_Handle hPhy, uint32_t reg, uint16_t val)
 Write PHY register. More...
 
int32_t EnetPhy_rmwReg (EnetPhy_Handle hPhy, uint32_t reg, uint16_t mask, uint16_t val)
 Read-modify-write PHY register. More...
 
int32_t EnetPhy_readExtReg (EnetPhy_Handle hPhy, uint32_t reg, uint16_t *val)
 Read PHY extended register. More...
 
int32_t EnetPhy_writeExtReg (EnetPhy_Handle hPhy, uint32_t reg, uint16_t val)
 Write PHY extended register. More...
 
int32_t EnetPhy_rmwExtReg (EnetPhy_Handle hPhy, uint32_t reg, uint16_t mask, uint16_t val)
 Read-modify-write PHY extended register. More...
 
int32_t EnetPhy_readC45Reg (EnetPhy_Handle hPhy, uint8_t mmd, uint32_t reg, uint16_t *val)
 Read PHY register using Clause-45 frame. More...
 
int32_t EnetPhy_writeC45Reg (EnetPhy_Handle hPhy, uint8_t mmd, uint32_t reg, uint16_t val)
 Write PHY register using Clause-45 frame. More...
 
int32_t EnetPhy_rmwC45Reg (EnetPhy_Handle hPhy, uint8_t mmd, uint32_t reg, uint16_t mask, uint16_t val)
 Read-modify-write PHY register using Clause-45 frame. More...
 
void EnetPhy_printRegs (EnetPhy_Handle hPhy)
 Print all PHY registers. More...