Time synchronization configuration structure.
Data Fields | |
uint8_t | domainNumber [TS_NUM_DOMAINS] |
uint32_t | syncOut_sync0Start |
uint32_t | syncOut_sync0PWidth |
TimeSync_SyncLossCallBack_t | timeSyncSyncLossCallBackfn |
TimeSync_stackResetCallback_t | ptpDrvStackReset |
int8_t | logPDelReqPktInterval |
int8_t | logSyncInterval |
int8_t | logAnnounceSendInterval |
int8_t | logAnnounceRcptTimeoutInterval |
uint32_t | pDelReqPktInterval |
uint32_t | syncSendInterval |
uint32_t | announceSendInterval |
uint32_t | announceRcptTimeoutInterval |
deviceConfig | config |
netWorkProtType | protocol |
delayType | type |
uint32_t | txIntNum |
uint16_t | asymmetryCorrection [ICSS_EMAC_MAX_PORTS_PER_INSTANCE] |
uint32_t | pdelayBurstInterval |
uint8_t | pdelayBurstNumPkts |
uint8_t | clockIdentity [8] |
uint32_t | sync0_interval |
uint8_t | hsrEnabled |
uint8_t | ll_has_hsrTag |
uint8_t | custom_tx_api |
uint8_t | timestamp_from_shared_ram |
uint8_t | emac_mode |
uint8_t | frame_offset |
uint32_t | tickPeriod |
uint32_t | rxPhyLatency |
uint32_t | txPhyLatency |
TimeSync_master_params_t | masterParams |
uint8_t TimeSync_Config_t::domainNumber[TS_NUM_DOMAINS] |
List of 802.1AS-rev domainNumbers
uint32_t TimeSync_Config_t::syncOut_sync0Start |
SYNCOUT sync0 start time
uint32_t TimeSync_Config_t::syncOut_sync0PWidth |
SYNCOUT sync0 pulse width
TimeSync_SyncLossCallBack_t TimeSync_Config_t::timeSyncSyncLossCallBackfn |
TimeSync_stackResetCallback_t TimeSync_Config_t::ptpDrvStackReset |
int8_t TimeSync_Config_t::logPDelReqPktInterval |
PDelay Request interval. Actual value is 2^value seconds
int8_t TimeSync_Config_t::logSyncInterval |
Sync send interval. Actual value is 2^value seconds
int8_t TimeSync_Config_t::logAnnounceSendInterval |
Announce send interval. Actual value is 2^value seconds
int8_t TimeSync_Config_t::logAnnounceRcptTimeoutInterval |
Announce receipt timeout interval. Actual value is 2^value seconds
uint32_t TimeSync_Config_t::pDelReqPktInterval |
Delay Request/PDelay Request interval. Mapped here from logPDelReqPktInterval Value in milliseconds
uint32_t TimeSync_Config_t::syncSendInterval |
Log of sync send interval. Mapped here from logSyncInterval value in microseconds
uint32_t TimeSync_Config_t::announceSendInterval |
Log of Announce send interval. Mapped here from logAnnounceSendInterval value in milliseconds
uint32_t TimeSync_Config_t::announceRcptTimeoutInterval |
Log of Announce receipt timeout interval. Min value of 3 value in milliseconds
deviceConfig TimeSync_Config_t::config |
Whether clock is OC or TC or both
netWorkProtType TimeSync_Config_t::protocol |
Packet type in which PTP is encapsulated
delayType TimeSync_Config_t::type |
Which type of Measurement scheme. E2E or P2P
uint32_t TimeSync_Config_t::txIntNum |
PTP Frame Tx Interrupt number
uint16_t TimeSync_Config_t::asymmetryCorrection[ICSS_EMAC_MAX_PORTS_PER_INSTANCE] |
Delay asymmetry correction value for both ports
uint32_t TimeSync_Config_t::pdelayBurstInterval |
In a Pdelay request burst packets are sent at this interval value in miliseconds
uint8_t TimeSync_Config_t::pdelayBurstNumPkts |
In a Pdelay request burst these many frames are sent
uint8_t TimeSync_Config_t::clockIdentity[8] |
Clock Identity = MAC ID + Protocol Identifier
uint32_t TimeSync_Config_t::sync0_interval |
ICSS generates a periodic pulse, can be configured from 1ms to 1s. When the interval is configured to 1s it becomes the 1PPS signal but has been kept to make it familiar
uint8_t TimeSync_Config_t::hsrEnabled |
Whether HSR is enabled or not
uint8_t TimeSync_Config_t::ll_has_hsrTag |
This field is only applicable to HSR frames. This is set to 1 if link local frames carry HSR tag By default this is set to 0 which means no HSR tag for Peer delay request/response frames. It Can be overridden from application (see HSR/PRP example) This gets over ridden in the driver once the peer sends delay request response frames
uint8_t TimeSync_Config_t::custom_tx_api |
Set to 1 if a customized Tx API is being used
uint8_t TimeSync_Config_t::timestamp_from_shared_ram |
Set to 1 if Rx timestamps are being read from ICSS shared RAM, a value of 0 indicates that timestamps are appended to the PTP frames being received in L3 RAM
uint8_t TimeSync_Config_t::emac_mode |
Set this to 1 to configure PTP to EMAC mode which means no bridge delay computation and forwarding
uint8_t TimeSync_Config_t::frame_offset |
All PTP packet offsets are w.r.t PTP Layer 3 packets an offset variable is hence used to calculate actual offset based on whether the configuration is E2E + L3 or P2P + L2
uint32_t TimeSync_Config_t::tickPeriod |
uint32_t TimeSync_Config_t::rxPhyLatency |
uint32_t TimeSync_Config_t::txPhyLatency |
TimeSync_master_params_t TimeSync_Config_t::masterParams |
Grand master parameters like priority 1, priority 2 etc. Populated in Announce frame