AM243x MCU+ SDK  08.03.00
enet_mod_mdio.h File Reference

Introduction

This file contains the type definitions and helper macros for the Enet MDIO module.

Go to the source code of this file.

Data Structures

struct  EnetMdio_C22ReadInArgs
 Input args for ENET_MDIO_IOCTL_C22_READ command. More...
 
struct  EnetMdio_C45ReadInArgs
 Input args for ENET_MDIO_IOCTL_C45_READ command. More...
 
struct  EnetMdio_C22WriteInArgs
 Input args for ENET_MDIO_IOCTL_C22_WRITE command. More...
 
struct  EnetMdio_C45WriteInArgs
 Input args for ENET_MDIO_IOCTL_C45_WRITE command. More...
 

Macros

#define ENET_MDIO_FEAT_CLAUSE45   (ENET_BIT(0U))
 MDIO feature mask for Clause-45 support. More...
 
#define ENET_MDIO_FEAT_PHY_MONITOR   (ENET_BIT(1U))
 MDIO feature mask for PHY state change monitoring. More...
 
#define ENET_MDIO_PUBLIC_IOCTL(x)
 Helper macro to create IOCTL commands for MDIO module. More...
 
#define ENET_MDIO_PHY_ADDR_MASK(addr)   (ENET_BIT(addr))
 Create a MDIO PHY mask from a PHY address. More...
 
#define ENET_MDIO_IS_PHY_ADDR_SET(mask, addr)   (((mask) & ENET_BIT(addr)) != 0U)
 Check if the corresponding PHY address mask is set. More...
 
#define ENET_MDIO_PHY_ADDR_MASK_NONE   (0x00000000U)
 MDIO PHY address mask for no PHYs present. More...
 
#define ENET_MDIO_PHY_ADDR_MASK_ALL   (0xFFFFFFFFU)
 MDIO PHY address mask for all PHYs present. More...
 
#define ENET_MDIO_PHY_CNT_MAX   (31U)
 Maximum number of PHYs supported on the MDIO bus. More...
 

Enumerations

enum  EnetMdio_Ioctl {
  ENET_MDIO_IOCTL_GET_VERSION = ENET_MDIO_PUBLIC_IOCTL(0U), ENET_MDIO_IOCTL_PRINT_REGS = ENET_MDIO_PUBLIC_IOCTL(1U), ENET_MDIO_IOCTL_IS_ALIVE = ENET_MDIO_PUBLIC_IOCTL(2U), ENET_MDIO_IOCTL_IS_LINKED = ENET_MDIO_PUBLIC_IOCTL(3U),
  ENET_MDIO_IOCTL_IS_POLL_ENABLED = ENET_MDIO_PUBLIC_IOCTL(4U), ENET_MDIO_IOCTL_C22_READ = ENET_MDIO_PUBLIC_IOCTL(5U), ENET_MDIO_IOCTL_C22_WRITE = ENET_MDIO_PUBLIC_IOCTL(6U), ENET_MDIO_IOCTL_C45_READ = ENET_MDIO_PUBLIC_IOCTL(7U),
  ENET_MDIO_IOCTL_C45_WRITE = ENET_MDIO_PUBLIC_IOCTL(8U), ENET_MDIO_IOCTL_C22_ASYNC_READ_TRIGGER = ENET_MDIO_PUBLIC_IOCTL(9U), ENET_MDIO_IOCTL_C22_ASYNC_READ_COMPLETE = ENET_MDIO_PUBLIC_IOCTL(10U), ENET_MDIO_IOCTL_C22_ASYNC_WRITE_TRIGGER = ENET_MDIO_PUBLIC_IOCTL(11U),
  ENET_MDIO_IOCTL_C22_ASYNC_WRITE_COMPLETE = ENET_MDIO_PUBLIC_IOCTL(12U), ENET_MDIO_IOCTL_C45_ASYNC_READ_TRIGGER = ENET_MDIO_PUBLIC_IOCTL(13U), ENET_MDIO_IOCTL_C45_ASYNC_READ_COMPLETE = ENET_MDIO_PUBLIC_IOCTL(14U), ENET_MDIO_IOCTL_C45_ASYNC_WRITE_TRIGGER = ENET_MDIO_PUBLIC_IOCTL(15U),
  ENET_MDIO_IOCTL_C45_ASYNC_WRITE_COMPLETE = ENET_MDIO_PUBLIC_IOCTL(16U), ENET_MDIO_IOCTL_ENABLE_STATE_MACHINE = ENET_MDIO_PUBLIC_IOCTL(17U)
}
 MDIO IOCTL commands. More...
 
enum  EnetMdio_Group { ENET_MDIO_GROUP_0 = 0U, ENET_MDIO_GROUP_1, ENET_MDIO_GROUP_NUM }
 MDIO user group. More...
 
enum  EnetMdio_FrameFmt { ENET_MDIO_FRAME_FMT_C22 = 0U, ENET_MDIO_FRAME_FMT_C45 }
 Frame format. More...
 
enum  EnetMdio_C45Mmd {
  ENET_MDIO_MMD_PMA_PMD = 1U, ENET_MDIO_MMD_WIS = 2U, ENET_MDIO_MMD_PCS = 3U, ENET_MDIO_MMD_PHY_XS = 4U,
  ENET_MDIO_MMD_DTE_XS = 5U, ENET_MDIO_MMD_VENDOR_1 = 30U, ENET_MDIO_MMD_VENDOR_2 = 31U
}
 Clause-45 MDIO Manageable Device (MMD) addresses. More...