The SOC driver provides API to configure SOC specific features like clocks.
Features Supported
- API to enable/disable a module clock
- API to set clock frequency for module
- Generic utility API like get CPU clock, get core name string, control module MMR lock/unlock API
- Address Translation APIs for all the R5F cores
- SOC Software Warm Reset/POR Reset APIs
SysConfig Features
- SOC driver is integrated with each of the drivers. User need not perform any explicit configuration for this driver
Features NOT Supported
NA
Important Usage Guidelines
- Most of these APIs are already integrated with SysConfig tool and the generated code does the required call to enable a module, set the required clock and so on. User need to use these APIs in their application only for exceptional scenarios.
- All MCU domain resets act as a master reset to the whole device. (MAIN and MCU domains)
- MAIN domain resets will only reset the MAIN domain.
- Please refer "Reset" chapter in techical reference manual for more details.
Example Usage
Include the below file to access the APIs
Get Core Name String
Get CPU Clock Frequency
uint64_t cpuClockRate;
DebugP_log(
"CPU Clock Frequency: %u\r\n", cpuClockRate);
API
APIs for SOC Specific Functions