For more details and example usage, see SOC
Functions | |
int32_t | SOC_moduleClockEnable (uint32_t moduleId, uint32_t enable) |
Enable clock to specified module. More... | |
int32_t | SOC_moduleSetClockFrequency (uint32_t moduleId, uint32_t clkId, uint64_t clkRate) |
Set module clock to specified frequency. More... | |
int32_t | SOC_moduleGetClockFrequency (uint32_t moduleId, uint32_t clkId, uint64_t *clkRate) |
Get module clock frequency. More... | |
const char * | SOC_getCoreName (uint16_t coreId) |
Convert a core ID to a user readable name. More... | |
uint64_t | SOC_getSelfCpuClk (void) |
Get the clock frequency in Hz of the CPU on which the driver is running. More... | |
void | SOC_controlModuleLockMMR (uint32_t domainId, uint32_t partition) |
Lock control module partition to prevent writes into control MMRs. More... | |
void | SOC_controlModuleUnlockMMR (uint32_t domainId, uint32_t partition) |
Unlock control module partition to allow writes into control MMRs. More... | |
void | SOC_setEpwmTbClk (uint32_t epwmInstance, uint32_t enable) |
Enable or disable ePWM time base clock from Control MMR. More... | |
uint64_t | SOC_virtToPhy (void *virtAddr) |
SOC Virtual (CPU) to Physical address translation function. More... | |
void * | SOC_phyToVirt (uint64_t phyAddr) |
Physical to Virtual (CPU) address translation function. More... | |
void | SOC_setDevStat (uint32_t bootMode) |
Change boot mode by setting devstat register. More... | |
uint32_t | SOC_isR5FDualCoreMode (CSL_ArmR5CPUInfo *cpuInfo) |
Return R5SS supporting single or dual core mode. More... | |
void | SOC_generateSwWarmResetMainDomain (void) |
Generate SW Warm Reset Main Domain. More... | |
void | SOC_generateSwPORResetMainDomain (void) |
Generate SW POR Reset Main Domain. More... | |
uint32_t | SOC_getWarmResetCauseMainDomain (void) |
Get the reset reason source for Main Domain. More... | |
void | SOC_generateSwWarmResetMcuDomain (void) |
Generate SW WARM Reset Mcu Domain. More... | |
void | SOC_generateSwWarmResetMainDomainFromMcuDomain (void) |
Generate SW WARM Reset Main Domain from Mcu Domain. More... | |
void | SOC_generateSwPORResetMainDomainFromMcuDomain (void) |
Generate SW POR Reset Main Domain from Mcu Domain. More... | |
uint32_t | SOC_getWarmResetCauseMcuDomain (void) |
Get the reset reason source for Mcu Domain. More... | |
void | SOC_clearResetCauseMainMcuDomain (uint32_t resetCause) |
Clears reason for Warm and Main/Mcu Domain Power On Resets. CTRLMMR_RST_SRC is just a mirror of CTRLMMR_MCU_RST_SRC register. It is read only. So we need to write 1 to CTRLMMR_MCU_RST_SRC to clear the reset reason. More... | |
Macros | |
#define | SOC_BOOTMODE_MMCSD (0X36C3) |
Switch value for SD card boot mode. More... | |
SOC Domain ID | |
#define | SOC_DOMAIN_ID_MAIN (0U) |
#define | SOC_DOMAIN_ID_MCU (1U) |
#define SOC_DOMAIN_ID_MAIN (0U) |
#define SOC_DOMAIN_ID_MCU (1U) |
#define SOC_BOOTMODE_MMCSD (0X36C3) |
Switch value for SD card boot mode.
int32_t SOC_moduleClockEnable | ( | uint32_t | moduleId, |
uint32_t | enable | ||
) |
Enable clock to specified module.
moduleId | [in] see tisci_devices for list of device ID's |
enable | [in] 1: enable clock to the module, 0: disable clock to the module |
int32_t SOC_moduleSetClockFrequency | ( | uint32_t | moduleId, |
uint32_t | clkId, | ||
uint64_t | clkRate | ||
) |
Set module clock to specified frequency.
moduleId | [in] see tisci_devices for list of module ID's |
clkId | [in] see tisci_clocks for list of clocks associated with the specified module ID |
clkRate | [in] Frequency to set in Hz |
int32_t SOC_moduleGetClockFrequency | ( | uint32_t | moduleId, |
uint32_t | clkId, | ||
uint64_t * | clkRate | ||
) |
Get module clock frequency.
moduleId | [in] see tisci_devices for list of module ID's |
clkId | [in] see tisci_clocks for list of clocks associated with the specified module ID |
clkRate | [out] Frequency of the clock |
const char* SOC_getCoreName | ( | uint16_t | coreId | ) |
Convert a core ID to a user readable name.
coreId | [in] see CSL_CoreID |
uint64_t SOC_getSelfCpuClk | ( | void | ) |
Get the clock frequency in Hz of the CPU on which the driver is running.
void SOC_controlModuleLockMMR | ( | uint32_t | domainId, |
uint32_t | partition | ||
) |
Lock control module partition to prevent writes into control MMRs.
domainId | [in] See SOC_DomainId_t |
partition | [in] Partition number to unlock |
void SOC_controlModuleUnlockMMR | ( | uint32_t | domainId, |
uint32_t | partition | ||
) |
Unlock control module partition to allow writes into control MMRs.
domainId | [in] See SOC_DomainId_t |
partition | [in] Partition number to unlock |
void SOC_setEpwmTbClk | ( | uint32_t | epwmInstance, |
uint32_t | enable | ||
) |
Enable or disable ePWM time base clock from Control MMR.
epwmInstance | [in] ePWM instance number [0 - (CSL_EPWM_PER_CNT-1)] |
enable | [in] TRUE to enable and FALSE to disable |
uint64_t SOC_virtToPhy | ( | void * | virtAddr | ) |
SOC Virtual (CPU) to Physical address translation function.
virtAddr | [IN] Virtual/CPU address |
void* SOC_phyToVirt | ( | uint64_t | phyAddr | ) |
Physical to Virtual (CPU) address translation function.
phyAddr | [IN] Physical address |
void SOC_setDevStat | ( | uint32_t | bootMode | ) |
Change boot mode by setting devstat register.
bootMode | [IN] Boot mode switch value |
uint32_t SOC_isR5FDualCoreMode | ( | CSL_ArmR5CPUInfo * | cpuInfo | ) |
Return R5SS supporting single or dual core mode.
cpuInfo | [IN] Pointer to the CSL_ArmR5CPUInfo struct. |
void SOC_generateSwWarmResetMainDomain | ( | void | ) |
Generate SW Warm Reset Main Domain.
void SOC_generateSwPORResetMainDomain | ( | void | ) |
Generate SW POR Reset Main Domain.
uint32_t SOC_getWarmResetCauseMainDomain | ( | void | ) |
Get the reset reason source for Main Domain.
void SOC_generateSwWarmResetMcuDomain | ( | void | ) |
Generate SW WARM Reset Mcu Domain.
void SOC_generateSwWarmResetMainDomainFromMcuDomain | ( | void | ) |
Generate SW WARM Reset Main Domain from Mcu Domain.
void SOC_generateSwPORResetMainDomainFromMcuDomain | ( | void | ) |
Generate SW POR Reset Main Domain from Mcu Domain.
uint32_t SOC_getWarmResetCauseMcuDomain | ( | void | ) |
Get the reset reason source for Mcu Domain.
void SOC_clearResetCauseMainMcuDomain | ( | uint32_t | resetCause | ) |
Clears reason for Warm and Main/Mcu Domain Power On Resets. CTRLMMR_RST_SRC is just a mirror of CTRLMMR_MCU_RST_SRC register. It is read only. So we need to write 1 to CTRLMMR_MCU_RST_SRC to clear the reset reason.
resetCause | [IN] Reset reason value to clear. |