AM243x MCU+ SDK  08.02.00
TLV2_TAG Struct Reference

Detailed Description

TLV2 tag

Data Fields

uint8_t type
 
uint8_t mac_length
 
uint8_t red_mac [ETHER_ADDR_LEN]
 

Field Documentation

◆ type

uint8_t TLV2_TAG::type

Source node identifier set to 30 if the source node is a RedBox

◆ mac_length

uint8_t TLV2_TAG::mac_length

Length of the following MAC address in octets

◆ red_mac

uint8_t TLV2_TAG::red_mac[ETHER_ADDR_LEN]

MAC addresses used by the RedBox on its interlink