AM243x MCU+ SDK  08.02.00

Introduction

Profinet Device FWHAL(Firmware and Hardware Abstraction Layer) APIs implement the key interface between Profinet firmware and slave stack.

Sub Modules

 CPM/PPM Management APIs
 
 DCP Filter APIs
 
 Isochronous Mode APIs
 
 Legacy Startup APIs
 
 MRP APIs
 
 Multicast Filter Table APIs
 
 PTCP APIs
 
 Phase Management APIs
 
 Triple buffer management APIs
 
 Watchdog timer APIs
 

Data Structures

struct  t_listIndex
 
struct  t_rtcMemBuff
 

Functions

void PN_registerPpmCall (PN_Handle pnHandle, pnCallBack_t callBack)
 Registers callback function required for PPM processing. More...
 
void PN_registerCpmCall (PN_Handle pnHandle, pnCallBack_t callBack)
 Registers callback function required for CPM processing. More...
 
void PN_registerStatCall (PN_Handle pnHandle, pnCallBack_t callBack)
 Registers callback function required for Stat processing. More...
 
void PN_clearPruIRQ (PRUICSS_HwAttrs const *pruicssHwAttrs, uint8_t irq_num)
 
int32_t PN_setBaseClock (PN_Handle pnHandle, uint16_t factor)
 Sets Profinet base clock in multiples of 31.25us. More...
 

Macros

#define SHADOW_LIST   0
 
#define ACTIVE_LIST   1
 
#define HALFSIZE   4
 

Macro Definition Documentation

◆ SHADOW_LIST

#define SHADOW_LIST   0

◆ ACTIVE_LIST

#define ACTIVE_LIST   1

◆ HALFSIZE

#define HALFSIZE   4

Function Documentation

◆ PN_registerPpmCall()

void PN_registerPpmCall ( PN_Handle  pnHandle,
pnCallBack_t  callBack 
)

Registers callback function required for PPM processing.

Parameters
pnHandleProfinet Handle
[in]callBackCallback function pointer

◆ PN_registerCpmCall()

void PN_registerCpmCall ( PN_Handle  pnHandle,
pnCallBack_t  callBack 
)

Registers callback function required for CPM processing.

Parameters
pnHandleProfinet Handle
[in]callBackCallback function pointer

◆ PN_registerStatCall()

void PN_registerStatCall ( PN_Handle  pnHandle,
pnCallBack_t  callBack 
)

Registers callback function required for Stat processing.

Parameters
pnHandleProfinet Handle
[in]callBackCallback function pointer

◆ PN_clearPruIRQ()

void PN_clearPruIRQ ( PRUICSS_HwAttrs const *  pruicssHwAttrs,
uint8_t  irq_num 
)

◆ PN_setBaseClock()

int32_t PN_setBaseClock ( PN_Handle  pnHandle,
uint16_t  factor 
)

Sets Profinet base clock in multiples of 31.25us.

Parameters
[in]pnHandleProfinet Handle
factorClock send factor: min value 8, max value 128
Return values
Slotnumber (>=0)
<0if failure

Variable Documentation

◆ pRtcConfig

uint32_t pRtcConfig

Stores PRUSS DataRAM0

◆ ocmcBaseAddress

uint32_t ocmcBaseAddress

Stores the OCMC Baseaddress