AM243x MCU+ SDK  08.02.00
enet_osal.h File Reference

Introduction

This file contains the OSAL API of the Enet driver.

Go to the source code of this file.

Data Structures

struct  EnetOsal_Cfg
 Enet OSAL configuration paramters. More...
 

Typedefs

typedef uintptr_t(* EnetOsal_DisableAllIntr) (void)
 Enet OSAL intr disable function prototype. More...
 
typedef void(* EnetOsal_RestoreAllIntr) (uintptr_t cookie)
 Enet OSAL intr restore function prototype. More...
 
typedef void(* EnetOsal_RestoreIntr) (uint32_t coreIntrNum)
 Enet OSAL intr restore function prototype. More...
 
typedef void(* EnetOsal_DisableIntr) (uint32_t coreIntrNum)
 Enet OSAL intr disable function prototype. More...
 
typedef void(* EnetOsal_Isr) (uintptr_t arg)
 Enet OSAL ISR callback function prototype. More...
 
typedef void *(* EnetOsal_RegisterIntr) (EnetOsal_Isr isrFxn, uint32_t coreIntrNum, uint32_t intrPriority, uint32_t triggerType, void *arg)
 Enet OSAL ISR register function prototype. More...
 
typedef void(* EnetOsal_UnregisterIntr) (void *hHwi)
 Enet OSAL ISR unregister function prototype. More...
 
typedef void *(* EnetOsal_CreateMutex) (void)
 Enet OSAL mutex create function prototype to protect critical section. More...
 
typedef void(* EnetOsal_DeleteMutex) (void *hMutex)
 Enet OSAL mutex delete function prototype. More...
 
typedef void(* EnetOsal_LockMutex) (void *hMutex)
 Enet OSAL mutex lock function prototype. More...
 
typedef void(* EnetOsal_UnlockMutex) (void *hMutex)
 Enet OSAL mutex lock function prototype. More...
 
typedef bool(* EnetOsal_IsCacheCoherent) (void)
 Enet OSAL cache coherency check function prototype. More...
 
typedef void(* EnetOsal_CacheInv) (const void *addr, int32_t size)
 Enet OSAL cache invalidate function prototype. More...
 
typedef void(* EnetOsal_CacheWb) (const void *addr, int32_t size)
 Enet OSAL cache writeback function prototype. More...
 
typedef void(* EnetOsal_CacheWbInv) (const void *addr, int32_t size)
 Enet OSAL cache writeback invalidate function prototype. More...
 
typedef uint32_t(* EnetOsal_TimerRead) (void)
 Enet OSAL timer read function prototype. More...
 

Enumerations

enum  EnetOSAL_armGicTrigType_t {
  ENETOSAL_ARM_GIC_TRIG_TYPE_LEVEL = 1, ENETOSAL_ARM_GIC_TRIG_TYPE_EDGE = 2, ENETOSAL_ARM_GIC_TRIG_TYPE_HIGH_LEVEL = 3, ENETOSAL_ARM_GIC_TRIG_TYPE_LOW_LEVEL = 4,
  ENETOSAL_ARM_GIC_TRIG_TYPE_RISING_EDGE = 5, ENETOSAL_ARM_GIC_TRIG_TYPE_FALLING_EDGE = 6
}
 Enumerates the types different trigger types. Please refer to Section 4.3.13 Interrupt Configuration Registers, GICD_ICFGRn of ARM Generic Interrupt Controller Architecture version 2.0 Architecture Specification document for details. More...
 

Functions

void EnetOsal_init (const EnetOsal_Cfg *cfg)
 Initialize OSAL with provided configuration. More...
 
void EnetOsal_deinit (void)
 Deinitialize OSAL. More...
 
uintptr_t EnetOsal_disableAllIntr (void)
 Enet OSAL intr disable function prototype. More...
 
void EnetOsal_restoreAllIntr (uintptr_t cookie)
 Enet OSAL intr restore function prototype. More...
 
void * EnetOsal_registerIntr (EnetOsal_Isr isrFxn, uint32_t coreIntrNum, uint32_t intrPriority, uint32_t intrTrigType, void *arg)
 Register an ISR for an interrupt. More...
 
void EnetOsal_unregisterIntr (void *hHwi)
 Unregister an interrupt. More...
 
void EnetOsal_enableIntr (uint32_t coreIntrNum)
 Enable interrupt. More...
 
void EnetOsal_disableIntr (uint32_t coreIntrNum)
 Disable interrupt. More...
 
void * EnetOsal_createMutex (void)
 Create a mutex. More...
 
void EnetOsal_deleteMutex (void *hMutex)
 Delete a mutex. More...
 
void EnetOsal_lockMutex (void *hMutex)
 Lock a mutex. More...
 
void EnetOsal_unlockMutex (void *hMutex)
 Unlock a mutex. More...
 
void EnetOsal_cacheInv (const void *addr, int32_t size)
 Invalidate cache. More...
 
void EnetOsal_cacheWb (const void *addr, int32_t size)
 Write-back cache. More...
 
void EnetOsal_cacheWbInv (const void *addr, int32_t size)
 Write-back and invalidate cache. More...
 
uint32_t EnetOsal_timerGetDiff (uint32_t startTime)
 Get the time difference with respect to timestamp. More...
 
uint32_t EnetOsal_timerRead (void)
 Read current timer value. More...
 

Typedef Documentation

◆ EnetOsal_DisableAllIntr

typedef uintptr_t(* EnetOsal_DisableAllIntr) (void)

Enet OSAL intr disable function prototype.

Returns
Cookie to be passed back to enable interrupt function

◆ EnetOsal_RestoreAllIntr

typedef void(* EnetOsal_RestoreAllIntr) (uintptr_t cookie)

Enet OSAL intr restore function prototype.

Parameters
cookieThis is returned in disable interrupt function

◆ EnetOsal_RestoreIntr

typedef void(* EnetOsal_RestoreIntr) (uint32_t coreIntrNum)

Enet OSAL intr restore function prototype.

Parameters
coreIntrNumInterrupt to restore

◆ EnetOsal_DisableIntr

typedef void(* EnetOsal_DisableIntr) (uint32_t coreIntrNum)

Enet OSAL intr disable function prototype.

Parameters
coreIntrNumInterrupt to disable

◆ EnetOsal_Isr

typedef void(* EnetOsal_Isr) (uintptr_t arg)

Enet OSAL ISR callback function prototype.

Parameters
argApp data

◆ EnetOsal_RegisterIntr

typedef void*(* EnetOsal_RegisterIntr) (EnetOsal_Isr isrFxn, uint32_t coreIntrNum, uint32_t intrPriority, uint32_t triggerType, void *arg)

Enet OSAL ISR register function prototype.

Parameters
isrFxnISR callback fxn pointer
coreIntrNumCore interrupt number to register
intrPriorityPriority
triggerTypeinterrupt trigger type for ARM corepac as EnetOSAL_armGicTrigType_t
argArg that will be passed back in the ISR
Returns
Created Hwi handle

◆ EnetOsal_UnregisterIntr

typedef void(* EnetOsal_UnregisterIntr) (void *hHwi)

Enet OSAL ISR unregister function prototype.

Parameters
hHwiHwi handle

◆ EnetOsal_CreateMutex

typedef void*(* EnetOsal_CreateMutex) (void)

Enet OSAL mutex create function prototype to protect critical section.

Returns
Pointer to mutex object

◆ EnetOsal_DeleteMutex

typedef void(* EnetOsal_DeleteMutex) (void *hMutex)

Enet OSAL mutex delete function prototype.

Parameters
hMutexPointer to mutex object returned during create

◆ EnetOsal_LockMutex

typedef void(* EnetOsal_LockMutex) (void *hMutex)

Enet OSAL mutex lock function prototype.

Parameters
hMutexPointer to mutex object returned during create

◆ EnetOsal_UnlockMutex

typedef void(* EnetOsal_UnlockMutex) (void *hMutex)

Enet OSAL mutex lock function prototype.

Parameters
hMutexPointer to mutex object returned during create

◆ EnetOsal_IsCacheCoherent

typedef bool(* EnetOsal_IsCacheCoherent) (void)

Enet OSAL cache coherency check function prototype.

Returns
Whether cache is coherent or not

◆ EnetOsal_CacheInv

typedef void(* EnetOsal_CacheInv) (const void *addr, int32_t size)

Enet OSAL cache invalidate function prototype.

Parameters
addrStart address of the cache line/s
sizeSize (in bytes) of the memory to invalidate

◆ EnetOsal_CacheWb

typedef void(* EnetOsal_CacheWb) (const void *addr, int32_t size)

Enet OSAL cache writeback function prototype.

Parameters
addrStart address of the cache line/s
sizeSize (in bytes) of the memory to be written back

◆ EnetOsal_CacheWbInv

typedef void(* EnetOsal_CacheWbInv) (const void *addr, int32_t size)

Enet OSAL cache writeback invalidate function prototype.

Parameters
addrStart address of the cache line/s
sizeSize (in bytes) of the memory to be written back

◆ EnetOsal_TimerRead

typedef uint32_t(* EnetOsal_TimerRead) (void)

Enet OSAL timer read function prototype.

Returns
Timer's read value

Enumeration Type Documentation

◆ EnetOSAL_armGicTrigType_t

Enumerates the types different trigger types. Please refer to Section 4.3.13 Interrupt Configuration Registers, GICD_ICFGRn of ARM Generic Interrupt Controller Architecture version 2.0 Architecture Specification document for details.

Enumerator
ENETOSAL_ARM_GIC_TRIG_TYPE_LEVEL 

Corresponding interrupt is level sensitive

ENETOSAL_ARM_GIC_TRIG_TYPE_EDGE 

Corresponding interrupt is edge sensitive

ENETOSAL_ARM_GIC_TRIG_TYPE_HIGH_LEVEL 

Coressponding interrupt is high level sensitive

ENETOSAL_ARM_GIC_TRIG_TYPE_LOW_LEVEL 

Coressponding interrupt is low level sensitive

ENETOSAL_ARM_GIC_TRIG_TYPE_RISING_EDGE 

Coressponding interrupt is rising edge sensitive

ENETOSAL_ARM_GIC_TRIG_TYPE_FALLING_EDGE 

Coressponding interrupt is falling edge sensitive

Function Documentation

◆ EnetOsal_init()

void EnetOsal_init ( const EnetOsal_Cfg cfg)

Initialize OSAL with provided configuration.

Initializes the Enet driver OSAL with the provided configuration. It's expected that all function pointers in the configuration are not NULL.

Parameters
cfgConfiguration parameters

◆ EnetOsal_deinit()

void EnetOsal_deinit ( void  )

Deinitialize OSAL.

Deinitializes the Enet driver OSAL by clearing the configuration previously set when calling EnetOsal_init().

◆ EnetOsal_disableAllIntr()

uintptr_t EnetOsal_disableAllIntr ( void  )

Enet OSAL intr disable function prototype.

Returns
Cookie to be passed back to enable interrupt function

◆ EnetOsal_restoreAllIntr()

void EnetOsal_restoreAllIntr ( uintptr_t  cookie)

Enet OSAL intr restore function prototype.

Parameters
cookieThis is returned in disable interrupt function

◆ EnetOsal_registerIntr()

void* EnetOsal_registerIntr ( EnetOsal_Isr  isrFxn,
uint32_t  coreIntrNum,
uint32_t  intrPriority,
uint32_t  intrTrigType,
void *  arg 
)

Register an ISR for an interrupt.

Parameters
isrFxnInterrupt service routine
coreIntrNumInterrupt number
intrPriorityInterrupt priority
intrTrigTypeInterrupt trigger type
argArgument to ISR function
Returns
Interrupt handle pointer

◆ EnetOsal_unregisterIntr()

void EnetOsal_unregisterIntr ( void *  hHwi)

Unregister an interrupt.

Parameters
hHwiInterrupt handle pointer

◆ EnetOsal_enableIntr()

void EnetOsal_enableIntr ( uint32_t  coreIntrNum)

Enable interrupt.

Parameters
coreIntrNumInterrupt number

◆ EnetOsal_disableIntr()

void EnetOsal_disableIntr ( uint32_t  coreIntrNum)

Disable interrupt.

Parameters
coreIntrNumInterrupt number

◆ EnetOsal_createMutex()

void* EnetOsal_createMutex ( void  )

Create a mutex.

Returns
Mutex handle pointer

◆ EnetOsal_deleteMutex()

void EnetOsal_deleteMutex ( void *  hMutex)

Delete a mutex.

Parameters
hMutexMutex handle pointer

◆ EnetOsal_lockMutex()

void EnetOsal_lockMutex ( void *  hMutex)

Lock a mutex.

Parameters
hMutexMutex handle pointer

◆ EnetOsal_unlockMutex()

void EnetOsal_unlockMutex ( void *  hMutex)

Unlock a mutex.

Parameters
hMutexMutex handle pointer

◆ EnetOsal_cacheInv()

void EnetOsal_cacheInv ( const void *  addr,
int32_t  size 
)

Invalidate cache.

Invalidates cache in a range of memory.

Parameters
addrStart address of the cache line(s)
sizeSize (in bytes) of the memory to invalidate

◆ EnetOsal_cacheWb()

void EnetOsal_cacheWb ( const void *  addr,
int32_t  size 
)

Write-back cache.

Writes back cache a range of memory from cache.

Parameters
addrStart address of the cache line(s)
sizeSize (in bytes) of the memory to be written back

◆ EnetOsal_cacheWbInv()

void EnetOsal_cacheWbInv ( const void *  addr,
int32_t  size 
)

Write-back and invalidate cache.

Writes back and invalidates a range of memory.

Parameters
addrStart address of the cache line/s
sizeSize (in bytes) of the memory to be written back

◆ EnetOsal_timerGetDiff()

uint32_t EnetOsal_timerGetDiff ( uint32_t  startTime)

Get the time difference with respect to timestamp.

Gets the difference between time value passed to this function and current time from timer.

Returns
Time difference

◆ EnetOsal_timerRead()

uint32_t EnetOsal_timerRead ( void  )

Read current timer value.

Returns
Timer's read value