#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
EI_API_CIP_NODE_T* pEI_API_CIP_NODE = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
uint16_t classId = 0x0064;
uint16_t getAttributesAllResponseInstanceLevel01[] = { 1, 2, 3, 4, 5 };
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:232
ETHIP_API uint32_t EI_API_CIP_createClass(T *pCipNode_p, uint16_t classId_p)
Create a CIP class.
Definition: EI_API_CIP_main.c:361
@ EI_API_CIP_eSC_GETATTRIBUTESALL
Definition: EI_API_def.h:114
@ EI_API_CIP_eSC_GETATTRSINGLE
Definition: EI_API_def.h:116
ETHIP_API uint32_t EI_API_CIP_addInstanceService(T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, EI_API_CIP_SService_t *pService_p)
Add one or more service/s to the class instance.
Definition: EI_API_CIP_main.c:1076
ETHIP_API uint32_t EI_API_CIP_createInstance(T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p)
Creates a CIP instance.
Definition: EI_API_CIP_main.c:905
ETHIP_API T * EI_API_CIP_NODE_new(void)
Create a new CIP node.
Definition: EI_API_CIP_main.c:69
EI_API_CIP_ESc_t code
Definition: EI_API_CIP.h:181
General service parameter collection.
Definition: EI_API_CIP.h:180