#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
EI_API_CIP_NODE_T* pEI_API_CIP_NODE = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
uint16_t classId;
uint16_t instanceId;
uint16_t attrId;
uint16_t assemblyInstanceId;
uint8_t srcBuffer[1];
...
classId = 0x70;
instanceId = 0x01;
attrId = 0x300;
uint8_t value = 0xFF;
assemblyInstanceId = 0x64;
...
if (size == sizeof(srcBuffer))
{
srcBuffer[0] = 0x5A;
}
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:232
ETHIP_API uint32_t EI_API_CIP_setAssemblyData(T *pCipNode_p, uint16_t assemblyInstanceId_p, void *pSourceBuffer_p, uint16_t sourceBufferLength_p)
Set assembly instance attribute data.
Definition: EI_API_CIP_main.c:5874
ETHIP_API uint32_t EI_API_CIP_addAssemblyMember(T *pCipNode_p, uint16_t assemblyInstanceId_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attributeId_p)
Add an member to an assembly member list.
Definition: EI_API_CIP_main.c:5484
ETHIP_API uint32_t EI_API_CIP_getAssemblySize(T *pCipNode_p, uint16_t assemblyInstanceId_p, uint16_t *pSize_p)
Get assembly instance attribute Size.
Definition: EI_API_CIP_main.c:5589
ETHIP_API uint32_t EI_API_CIP_createAssembly(T *pCipNode_p, uint16_t assemblyInstanceId_p, EI_API_CIP_EAr_t accessRule_p)
Create a new assembly instance.
Definition: EI_API_CIP_main.c:5348
ETHIP_API uint32_t EI_API_CIP_addClassService(T *pCipNode_p, uint16_t classId_p, EI_API_CIP_SService_t *pService_p)
Add service/s to the class.
Definition: EI_API_CIP_main.c:435
ETHIP_API uint32_t EI_API_CIP_createClass(T *pCipNode_p, uint16_t classId_p)
Create a CIP class.
Definition: EI_API_CIP_main.c:361
@ EI_API_CIP_eSC_GETATTRSINGLE
Definition: EI_API_def.h:116
@ EI_API_CIP_eSC_SETATTRSINGLE
Definition: EI_API_def.h:117
@ EI_API_CIP_eAR_GET_AND_SET
Definition: EI_API_def.h:131
@ EI_API_CIP_eEDT_USINT
Definition: EI_API_CIP.h:127
@ EI_API_CIP_eCDT_NO
Definition: EI_API_CIP.h:163
ETHIP_API uint32_t EI_API_CIP_createInstance(T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p)
Creates a CIP instance.
Definition: EI_API_CIP_main.c:905
ETHIP_API uint32_t EI_API_CIP_addInstanceAttr(T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, EI_API_CIP_SAttr_t *pAttr_p)
Add an attribute to an instance.
Definition: EI_API_CIP_main.c:1454
ETHIP_API uint32_t EI_API_CIP_setInstanceAttr(T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, EI_API_CIP_SAttr_t *pAttr_p)
Set instance attribute value only.
Definition: EI_API_CIP_main.c:2234
ETHIP_API T * EI_API_CIP_NODE_new(void)
Create a new CIP node.
Definition: EI_API_CIP_main.c:69
EI_API_CIP_EEdt_t edt
Definition: EI_API_CIP.h:194
EI_API_CIP_EAr_t accessRule
Definition: EI_API_CIP.h:196
uint16_t id
Definition: EI_API_CIP.h:193
EI_API_CIP_ECdt_t cdt
Definition: EI_API_CIP.h:195
uint16_t cdtSize
Definition: EI_API_CIP.h:198
void * pvValue
Definition: EI_API_CIP.h:200
General attribute parameter collection.
Definition: EI_API_CIP.h:192
EI_API_CIP_ESc_t code
Definition: EI_API_CIP.h:181
EI_API_CIP_CBService callback
Definition: EI_API_CIP.h:184
uint16_t getAttrAllResponseCnt
Definition: EI_API_CIP.h:182
General service parameter collection.
Definition: EI_API_CIP.h:180