uint32_t EI_API_ADP_setPortLogAnnounceInterval | ( | T * | pAdp_p, |
uint16_t | portLogAnnounceInterval_p | ||
) |
Set the PortLogAnnounceInterval of the timeSync object of the adapter (Instance Attribute ID: 14).
Function that sets the Port Log Announce Interval attribute of the adapter selected by parameter pAdp_p
. PortLogAnnounceInterval specifies the PTP announce interval between successive �Announce� messages issued by a master clock on each PTP port of the device. The units of the PortLogAnnounceInterval member are log base 2 seconds. The PortLogAnnounceInterval is uint16_t
type. It's limited to values between 0 and 4.
[in] | pAdp_p | Pointer to the adapter. |
[in] | portLogAnnounceInterval_p | uint16_t Value of PTP Announce frame interval |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |