uint32_t EI_API_ADP_setTimeSyncSupported | ( | T * | pAdp_p | ) |
Enable TimeSync Support.
Enable TimeSync Support. This function should only be used for EtherNet_IP TimeSync applications.
[in] | pAdp_p | Pointer to the adapter. |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |