uint32_t EI_API_ADP_setDomainNumber | ( | T * | pAdp_p, |
uint8_t | domainNumber_p | ||
) |
Set the DomainNumber of the timeSync object of the adapter (Instance Attribute ID: 18).
Function that sets the Domain number attribute of the timeSync object of the adapter selected by parameter pAdp_p
. DomainNumber specifies the PTP clock domain. The DomainNumber is uint8_t
type. It's limited to values between 0 and 127.
[in] | pAdp_p | Pointer to the adapter. |
[in] | domainNumber_p | uint8_t Domain number |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |