uint32_t EI_API_ADP_getDomainNumber | ( | T * | pAdp_p, |
uint8_t * | pDomainNumber_p | ||
) |
Get the DomainNumber attribute of the timeSync object (Instance Attribute ID: 18).
Function that returns the DomainNumber attribute by parameter pAdp_p
in output parameter pDomainNumber
.
[in] | pAdp_p | Pointer to the adapter. |
[out] | pDomainNumber_p | uint8_t pointer to DomainNumber of the adapter timeSync object specified by parameter pAdp_p . |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |