uint32_t EI_API_ADP_getHostName | ( | T * | pAdp_p, |
char * | pHostName_p | ||
) |
Get the host name (Instance Attribute ID: 6).
Function that returns a pointer to the host name of the adapter selected by parameter pAdp_p
.
[in] | pAdp_p | Pointer to the adapter. |
[out] | pHostName_p | Character array with host name. |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |