uint32_t EI_API_ADP_setQuickConnectEnabled | ( | T * | pAdp_p, |
bool | quickConnectEnabled_p | ||
) |
Set the current adapter QuickConnect state (Instance Attribute ID: 12).
This function sets the EtherNet/IP Adapter QuickConnect state.
Value | Description |
---|---|
0 | Disable |
1 | Enable |
[in] | pAdp_p | Pointer to the adapter. |
[in] | quickConnectEnabled_p | The QuickConnect state. |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |