#include <api/EI_API.h>
uint32_t errCode;
ETHIP_API uint32_t EI_API_ADP_loadMac(EIP_SLoadParameter *ptPara_p, uint8_t pruInstance)
Load and initialize EthernetIP firmware in PRU.
Definition: EI_API_ADP_main.c:103
ETHIP_API void EI_API_ADP_startFirmware(void)
Enable PRU firmware.
Definition: EI_API_ADP_main.c:177
uint8_t ai8uMacAddr[EIP_MAC_ADDR_LEN]
Definition: EI_API_ADP.h:164
Definition: EI_API_ADP.h:163