AM243x MCU+ SDK  08.01.00

Introduction

The CPSW MAC port module provides additional IOCTL commands than those supported by the generic Enet MAC Port API set.

CPSW MAC port clocks:

Features:

Compile-time configuration:

Data Structures

struct  CpswMacPort_TxShortIpgCfg
 Configuration of transmit short inter packet gap feature. More...
 
struct  CpswMacPort_PortTxShortIpgCfg
 MAC port's short gap configuration. More...
 
struct  CpswMacPort_InterVlanRoutingCfg
 Port interVLAN configuration parameters. More...
 
struct  CpswMacPort_FifoStats
 FIFO related statistics of a MAC port. More...
 
struct  CpswMacPort_IpTsCfg
 Port IP configuration for time synchronization events. More...
 
struct  CpswMacPort_TsEventCfg
 Port configuration for time synchronization. More...
 
struct  CpswMacPort_EnableTsEventInArgs
 Input args for CPSW_MACPORT_IOCTL_ENABLE_CPTS_EVENT. More...
 
struct  CpswMacPort_Cfg
 MAC port module configuration parameters. More...
 

Functions

void CpswMacPort_initCfg (CpswMacPort_Cfg *macPortCfg)
 Initialize CPSW MAC port configuration parameters. More...
 

Enumerations

enum  CpswMacPort_Ioctl { CPSW_MACPORT_IOCTL_GET_FIFO_STATS = CPSW_MACPORT_PUBLIC_IOCTL(0U), CPSW_MACPORT_IOCTL_ENABLE_CPTS_EVENT = CPSW_MACPORT_PUBLIC_IOCTL(1U), CPSW_MACPORT_IOCTL_DISABLE_CPTS_EVENT = CPSW_MACPORT_PUBLIC_IOCTL(2U) }
 CPSW MAC port IOCTL commands. More...
 
enum  CpswMacPort_InterVlanRouteId {
  CPSW_MACPORT_INTERVLAN_ROUTEID_FIRST, CPSW_MACPORT_INTERVLAN_ROUTEID_1 = CPSW_MACPORT_INTERVLAN_ROUTEID_FIRST, CPSW_MACPORT_INTERVLAN_ROUTEID_2, CPSW_MACPORT_INTERVLAN_ROUTEID_3,
  CPSW_MACPORT_INTERVLAN_ROUTEID_4, CPSW_MACPORT_INTERVLAN_ROUTEID_LAST = CPSW_MACPORT_INTERVLAN_ROUTEID_4
}
 MAC port interVLAN route identifier. More...
 

Macros

#define CPSW_MACPORT_PUBLIC_IOCTL(x)
 Helper macro to create IOCTL commands for CPSW MAC port module. More...
 

Macro Definition Documentation

◆ CPSW_MACPORT_PUBLIC_IOCTL

#define CPSW_MACPORT_PUBLIC_IOCTL (   x)
Value:
ENET_IOCTL_MACPORT_BASE | \
ENET_IOCTL_PER_CPSW | \
ENET_IOCTL_MIN(x))

Helper macro to create IOCTL commands for CPSW MAC port module.

Enumeration Type Documentation

◆ CpswMacPort_Ioctl

CPSW MAC port IOCTL commands.

Enumerator
CPSW_MACPORT_IOCTL_GET_FIFO_STATS 

Get MAC port FIFO statistics.

IOCTL parameters:

CPSW_MACPORT_IOCTL_ENABLE_CPTS_EVENT 

Enable Ethernet port CPTS event.

IOCTL parameters:

CPSW_MACPORT_IOCTL_DISABLE_CPTS_EVENT 

Disable Ethernet port CPTS event.

IOCTL parameters:

◆ CpswMacPort_InterVlanRouteId

MAC port interVLAN route identifier.

Enumerator
CPSW_MACPORT_INTERVLAN_ROUTEID_FIRST 

First interVLAN route Id

CPSW_MACPORT_INTERVLAN_ROUTEID_1 

InterVLAN route Id 1

CPSW_MACPORT_INTERVLAN_ROUTEID_2 

InterVLAN route Id 2

CPSW_MACPORT_INTERVLAN_ROUTEID_3 

InterVLAN route Id 3

CPSW_MACPORT_INTERVLAN_ROUTEID_4 

InterVLAN route Id 4

CPSW_MACPORT_INTERVLAN_ROUTEID_LAST 

Last interVLAN route Id

Function Documentation

◆ CpswMacPort_initCfg()

void CpswMacPort_initCfg ( CpswMacPort_Cfg macPortCfg)

Initialize CPSW MAC port configuration parameters.

Parameters
macPortCfgConfiguration parameters to be initialized
ENET_IOCTL_TYPE_PUBLIC
@ ENET_IOCTL_TYPE_PUBLIC
Definition: enet_ioctl.h:167