This file contains declarations of CSL APIs corresponding to the ePWM module. This also contains necessary structure, enum and macro definitions and APIs are consolidated to provide more functional APIs.
Programming sequence of EPWM is as follows:
Go to the source code of this file.
EPWM Output Channel | |
#define | EPWM_OUTPUT_CH_MIN (0U) |
#define | EPWM_OUTPUT_CH_A (EPWM_OUTPUT_CH_MIN) |
#define | EPWM_OUTPUT_CH_B (1U) |
#define | EPWM_OUTPUT_CH_MAX (EPWM_OUTPUT_CH_B) |
typedef uint32_t | Epwm_OutputCh_t |
Number of supported EPWM outputs in a single epwm channel. More... | |
EPWM Tb Counter Direction | |
#define | EPWM_TB_COUNTER_DIR_UP (PWMSS_EPWM_TBCTL_CTRMODE_UP_COUNT) |
#define | EPWM_TB_COUNTER_DIR_DOWN (PWMSS_EPWM_TBCTL_CTRMODE_DOWN_COUNT) |
#define | EPWM_TB_COUNTER_DIR_UP_DOWN (PWMSS_EPWM_TBCTL_CTRMODE_UP_DOWN_COUNT) |
#define | EPWM_TB_COUNTER_DIR_STOP (PWMSS_EPWM_TBCTL_CTRMODE_STOP_FREEZE) |
typedef uint32_t | Epwm_TbCounterDir_t |
Types of Time base counter direction modes. More... | |
EPWM Shadow register Control | |
#define | EPWM_SHADOW_REG_CTRL_ENABLE (PWMSS_EPWM_TBCTL_PRDLD_LOAD_FROM_SHADOW) |
#define | EPWM_SHADOW_REG_CTRL_DISABLE (PWMSS_EPWM_TBCTL_PRDLD_LOAD_IMMEDIATELY) |
typedef uint32_t | Epwm_ShadowRegCtrl_t |
Shadow register enable or disable control. More... | |
EPWM Counter directions after sync event | |
#define | EPWM_TB_CNT_DIR_AFT_SYNC_DOWN (PWMSS_EPWM_TBCTL_PHSDIR_COUNT_DOWN) |
#define | EPWM_TB_CNT_DIR_AFT_SYNC_UP (PWMSS_EPWM_TBCTL_PHSDIR_COUNT_UP) |
typedef uint32_t | Epwm_TbCntDirAftSync_t |
Counter directions after sync event. More... | |
EPWM Source of Synchronization output signal | |
#define | EPWM_TB_SYNC_OUT_EVT_SYNCIN (PWMSS_EPWM_TBCTL_SYNCOSEL_EPWMXSYNC) |
#define | EPWM_TB_SYNC_OUT_EVT_CNT_EQ_ZERO (PWMSS_EPWM_TBCTL_SYNCOSEL_CTR_0) |
#define | EPWM_TB_SYNC_OUT_EVT_CNT_EQ_CMP_B (PWMSS_EPWM_TBCTL_SYNCOSEL_CTR_CPMB) |
#define | EPWM_TB_SYNC_OUT_EVT_DISABLE (PWMSS_EPWM_TBCTL_SYNCOSEL_DISABLE_EPWMXSYNCO) |
typedef uint32_t | Epwm_TbSyncOutEvt_t |
Source of Synchronization output signal. More... | |
EPWM Flags to get the different types of time base status | |
#define | EPWM_TB_STS_CTR_MAX (PWMSS_EPWM_TBSTS_CTRMAX_MASK) |
#define | EPWM_TB_STS_SYNCI (PWMSS_EPWM_TBSTS_SYNCI_MASK) |
#define | EPWM_TB_STS_CTR_DIR (PWMSS_EPWM_TBSTS_CTRDIR_MASK) |
typedef uint32_t | Epwm_TbSts_t |
Flags to get the different types of time base status. More... | |
EPWM Emulation Mode | |
#define | EPWM_TB_EMU_MODE_STP_AFT_NEXT_CYCLE (PWMSS_EPWM_TBCTL_FREE_SOFT_STOP_AFTER_NEXT_CTR) |
#define | EPWM_TB_EMU_MODE_STP_AFT_COMPLETE_CYCLE (PWMSS_EPWM_TBCTL_FREE_SOFT_STOP_AFTER_CYCLE) |
#define | EPWM_TB_EMU_MODE_FREE_RUN (PWMSS_EPWM_TBCTL_FREE_SOFT_RUN2) |
typedef uint32_t | Epwm_TbEmuMode_t |
Emulation Mode. This selects the behaviour of the ePWM time-base counter during emulation events. More... | |
EPWM Comparator type | |
#define | EPWM_CC_CMP_MIN (0U) |
#define | EPWM_CC_CMP_A (EPWM_CC_CMP_MIN) |
#define | EPWM_CC_CMP_B (1U) |
#define | EPWM_CC_CMP_MAX (CSL_EPWM_CC_CMP_B) |
typedef uint32_t | Epwm_CcCmp_t |
EPWM Counter-Comparator registers(A and B) load mode | |
#define | EPWM_CC_CMP_LOAD_MODE_CNT_EQ_ZERO (PWMSS_EPWM_CMPCTL_LOADAMODE_CTR_0) |
#define | EPWM_CC_CMP_LOAD_MODE_CNT_EQ_PRD (PWMSS_EPWM_CMPCTL_LOADAMODE_CTR_PRD) |
#define | EPWM_CC_CMP_LOAD_MODE_CNT_EQ_ZERO_OR_PRD (PWMSS_EPWM_CMPCTL_LOADAMODE_CTR_0_OR_PRD) |
#define | EPWM_CC_CMP_LOAD_MODE_NO_LOAD (PWMSS_EPWM_CMPCTL_LOADAMODE_FREEZE) |
typedef uint32_t | Epwm_CcCmpLoadMode_t |
Counter-Comparator registers(A and B) load mode flags from shadow register. More... | |
EPWM Actions | |
#define | EPWM_AQ_ACTION_DONOTHING (PWMSS_EPWM_AQCTLA_ZRO_DISABLED) |
#define | EPWM_AQ_ACTION_LOW (PWMSS_EPWM_AQCTLA_ZRO_CLEAR) |
#define | EPWM_AQ_ACTION_HIGH (PWMSS_EPWM_AQCTLA_ZRO_SET) |
#define | EPQM_AQ_ACTION_TOLLGE (PWMSS_EPWM_AQCTLA_ZRO_TOGGLE) |
#define | EPWM_AQ_ACTION_TOLLGE (CSL_EPQM_AQ_ACTION_TOLLGE) |
typedef uint32_t | Epwm_AqAction_t |
Types of Actions that Action Qualifier can take on the Output when the supported counter compare event occurs. More... | |
EPWM output actions | |
#define | EPWM_AQ_SW_TRIG_OT_ACTION_DONOTHING (PWMSS_EPWM_AQSFRC_ACTSFA_DISABLED) |
#define | EPWM_AQ_SW_TRIG_OT_ACTION_LOW (PWMSS_EPWM_AQSFRC_ACTSFA_CLEAR) |
#define | EPWM_AQ_SW_TRIG_OT_ACTION_HIGH (PWMSS_EPWM_AQSFRC_ACTSFA_SET) |
#define | EPWM_AQ_SW_TRIG_OT_ACTION_TOGGLE (PWMSS_EPWM_AQSFRC_ACTSFA_TOGGLE) |
typedef uint32_t | Epwm_AqSwTrigOtAction_t |
Actions to be taken on the output, when Software triggered one time events will occur. More... | |
EPWM Continuous software forced actions | |
#define | EPWM_AQ_SW_TRIG_CONT_ACTION_NOEFFECT (PWMSS_EPWM_AQCSFRC_CSFA_DISABLED) |
#define | EPWM_AQ_SW_TRIG_CONT_ACTION_LOW (PWMSS_EPWM_AQCSFRC_CSFA_LOW_OUTPUT) |
#define | EPWM_AQ_SW_TRIG_CONT_ACTION_HIGH (PWMSS_EPWM_AQCSFRC_CSFA_HIGH_OUTPUT) |
#define | EPWM_AQ_SW_TRIG_CONT_ACTION_SW_DISBALED (PWMSS_EPWM_AQCSFRC_CSFA_NO_EFFECT) |
typedef uint32_t | Epwm_AqSwTrigContAction_t |
Types of Continuous software forced actions on output. More... | |
EPWM Software Force Active Register Reload | |
#define | EPWM_AQ_CSFRC_REG_RELOAD_CNT_EQ_ZRO (PWMSS_EPWM_AQSFRC_RLDCSF_CTR_0) |
#define | EPWM_AQ_CSFRC_REG_RELOAD_CNT_EQ_PRD (PWMSS_EPWM_AQSFRC_RLDCSF_CTR_PERIOD) |
#define | EPWM_AQ_CSFRC_REG_RELOAD_CNT_EQ_ZRO_OR_PRD (PWMSS_EPWM_AQSFRC_RLDCSF_CTR_0_OR_PERIOD) |
#define | EPWM_AQ_CSFRC_REG_RELOAD_IMMEDIATE (PWMSS_EPWM_AQSFRC_RLDCSF_IMMEDIATE) |
typedef uint32_t | Epwm_AqCsfrcRegReload_t |
Action Qualifier Software Force Active Register Reload From Shadow Options. More... | |
EPWM Dead Band Input Mode Control | |
#define | EPWM_DB_IN_MODE_A_RED_A_FED (PWMSS_EPWM_DBCTL_IN_MODE_SRC_ARED_AFED) |
#define | EPWM_DB_IN_MODE_B_RED_A_FED (PWMSS_EPWM_DBCTL_IN_MODE_SRC_BRED_AFED) |
#define | EPWM_DB_IN_MODE_A_RED_B_FED (PWMSS_EPWM_DBCTL_IN_MODE_SRC_ARED_BFED) |
#define | EPWM_DB_IN_MODE_B_RED_B_FED (PWMSS_EPWM_DBCTL_IN_MODE_SRC_BRED_BFED) |
typedef uint32_t | Epwm_DbInMode_t |
Dead Band Input Mode Control. This allows you to select the input source to the falling-edge and rising-edge delay. More... | |
EPWM Polarity Select Control | |
#define | EPWM_DB_POL_SEL_ACTV_HIGH (PWMSS_EPWM_DBCTL_POLSEL_ACTIVE_HIGH) |
#define | EPWM_DB_POL_SEL_ACTV_LOW_COMPLEMENTARY (PWMSS_EPWM_DBCTL_POLSEL_ACTIVE_LOW_COMPLEMENTARY) |
#define | EPWM_DB_POL_SEL_ACTV_HIGH_COMPLEMENTARY (PWMSS_EPWM_DBCTL_POLSEL_ACTIVE_HIGH_COMPLEMENTARY) |
#define | EPWM_DB_POL_SEL_ACTV_LOW (PWMSS_EPWM_DBCTL_POLSEL_ACTIVE_LOW) |
typedef uint32_t | Epwm_DbPolSel_t |
Polarity Select Control. This allows you to selectively invert one of the delayed signals before it is sent out of the dead-band sub-module. More... | |
EPWM Dead-band Output Mode Control | |
#define | EPWM_DB_OUT_MODE_BYPASS (PWMSS_EPWM_DBCTL_OUT_MODE_DISABLED) |
#define | EPWM_DB_OUT_MODE_NO_RED_B_FED (PWMSS_EPWM_DBCTL_OUT_MODE_DISABLE_RISING_EDGE) |
#define | EPWM_DB_OUT_MODE_A_RED_NO_FED (PWMSS_EPWM_DBCTL_OUT_MODE_DISABLE_FALLING_EDGE) |
#define | EPWM_DB_OUT_MODE_A_RED_B_FED (PWMSS_EPWM_DBCTL_OUT_MODE_ENABLED) |
typedef uint32_t | Epwm_DbOutMode_t |
Dead-band Output Mode Control. This allows you to selectively enable or bypass the dead-band generation for the falling-edge and rising-edge delay. More... | |
EPWM Chopping Clock Duty Cycle | |
#define | EPWM_CHP_DUTY_CYCLE_PERC_12PNT5 (PWMSS_EPWM_PCCTL_CHPDUTY_DUTY_12_5) |
#define | EPWM_CHP_DUTY_CYCLE_PERC_25 (PWMSS_EPWM_PCCTL_CHPDUTY_DUTY_25) |
#define | EPWM_CHP_DUTY_CYCLE_PERC_37PNT5 (PWMSS_EPWM_PCCTL_CHPDUTY_DUTY_37_5) |
#define | EPWM_CHP_DUTY_CYCLE_PERC_50_PER (PWMSS_EPWM_PCCTL_CHPDUTY_DUTY_50) |
#define | EPWM_CHP_DUTY_CYCLE_PERC_62PNT5 (PWMSS_EPWM_PCCTL_CHPDUTY_DUTY_62_5) |
#define | EPWM_CHP_DUTY_CYCLE_PERC_75 (PWMSS_EPWM_PCCTL_CHPDUTY_DUTY_75) |
#define | EPWM_CHP_DUTY_CYCLE_PERC_87PNT5 (PWMSS_EPWM_PCCTL_CHPDUTY_DUTY_87_5) |
typedef uint32_t | Epwm_ChpDutyCycle_t |
Chopping Clock Duty Cycle values. More... | |
EPWM Chopping Clock Frequency | |
#define | EPWM_CHP_CLK_FREQ_DIV_BY_1 (PWMSS_EPWM_PCCTL_CHPFREQ_DIV_1) |
#define | EPWM_CHP_CLK_FREQ_DIV_BY_2 (PWMSS_EPWM_PCCTL_CHPFREQ_DIV_2) |
#define | EPWM_CHP_CLK_FREQ_DIV_BY_3 (PWMSS_EPWM_PCCTL_CHPFREQ_DIV_3) |
#define | EPWM_CHP_CLK_FREQ_DIV_BY_4 (PWMSS_EPWM_PCCTL_CHPFREQ_DIV_4) |
#define | EPWM_CHP_CLK_FREQ_DIV_BY_5 (PWMSS_EPWM_PCCTL_CHPFREQ_DIV_5) |
#define | EPWM_CHP_CLK_FREQ_DIV_BY_6 (PWMSS_EPWM_PCCTL_CHPFREQ_DIV_6) |
#define | EPWM_CHP_CLK_FREQ_DIV_BY_7 (PWMSS_EPWM_PCCTL_CHPFREQ_DIV_7) |
#define | EPWM_CHP_CLK_FREQ_DIV_BY_8 (PWMSS_EPWM_PCCTL_CHPFREQ_DIV_8) |
typedef uint32_t | Epwm_ChpClkFreq_t |
Chopping Clock Frequency values . More... | |
EPWM One-Shot Pulse Width | |
#define | EPWM_CHP_OSHT_WIDTH_MIN (0U) |
#define | EPWM_CHP_OSHT_WIDTH_1XSYSOUT_BY_8 (CSL_EPWM_CHP_OSHT_WIDTH_MIN) |
#define | EPWM_CHP_OSHT_WIDTH_2XSYSOUT_BY_8 (1U) |
#define | EPWM_CHP_OSHT_WIDTH_3XSYSOUT_BY_8 (2U) |
#define | EPWM_CHP_OSHT_WIDTH_4XSYSOUT_BY_8 (3U) |
#define | EPWM_CHP_OSHT_WIDTH_5XSYSOUT_BY_8 (4U) |
#define | EPWM_CHP_OSHT_WIDTH_6XSYSOUT_BY_8 (5U) |
#define | EPWM_CHP_OSHT_WIDTH_7XSYSOUT_BY_8 (6U) |
#define | EPWM_CHP_OSHT_WIDTH_8XSYSOUT_BY_8 (7U) |
#define | EPWM_CHP_OSHT_WIDTH_9XSYSOUT_BY_8 (8U) |
#define | EPWM_CHP_OSHT_WIDTH_10XSYSOUT_BY_8 (9U) |
#define | EPWM_CHP_OSHT_WIDTH_11XSYSOUT_BY_8 (10U) |
#define | EPWM_CHP_OSHT_WIDTH_12XSYSOUT_BY_8 (11U) |
#define | EPWM_CHP_OSHT_WIDTH_13XSYSOUT_BY_8 (12U) |
#define | EPWM_CHP_OSHT_WIDTH_14XSYSOUT_BY_8 (13U) |
#define | EPWM_CHP_OSHT_WIDTH_15XSYSOUT_BY_8 (14U) |
#define | EPWM_CHP_OSHT_WIDTH_16XSYSOUT_BY_8 (15U) |
#define | EPWM_CHP_OSHT_WIDTH_MAX (CSL_EPWM_CHP_OSHT_WIDTH_16XSYSOUT_BY_8) |
typedef uint32_t | Epwm_ChpOshtWidth_t |
One-Shot Pulse Width values. More... | |
EPWM output action when a trip event occurs | |
#define | EPWM_TZ_TRIP_ACTION_TRI_STATE (PWMSS_EPWM_TZCTL_TZA_HIGH_IMPEDANCE) |
#define | EPWM_TZ_TRIP_ACTION_HIGH (PWMSS_EPWM_TZCTL_TZA_HIGH_STATE) |
#define | EPWM_TZ_TRIP_ACTION_LOW (PWMSS_EPWM_TZCTL_TZA_LOW_STATE) |
#define | EPWM_TZ_TRIP_ACTION_DO_NOTHING (PWMSS_EPWM_TZCTL_TZA_DO_NOTHING) |
typedef uint32_t | Epwm_TzTripAction_t |
Action to be taken on PWM output When a trip event occurs. More... | |
EPWM trip zone events | |
#define | EPWM_TZ_EVENT_MIN (0x0U) |
#define | EPWM_TZ_EVENT_ONE_SHOT (EPWM_TZ_EVENT_MIN) |
#define | EPWM_TZ_EVENT_CYCLE_BY_CYCLE (0x1U) |
#define | EPWM_TZ_EVENT_MAX (CSL_EPWM_TZ_EVENT_CYCLE_BY_CYCLE) |
typedef uint32_t | Epwm_TzEvent_t |
Type of trip zone events. More... | |
EPWM Trip zone status flags | |
#define | EPWM_TZ_STS_FLG_OST (PWMSS_EPWM_TZFLG_OST_MASK) |
#define | EPWM_TZ_STS_FLG_CBC (PWMSS_EPWM_TZFLG_CBC_MASK) |
#define | EPWM_TZ_STS_FLG_INT (PWMSS_EPWM_TZFLG_INT_MASK) |
typedef uint32_t | Epwm_TzStsFlg_t |
Trip zone status flags. More... | |
EPWM Interrupt (EPWMx_INT) Selection Options | |
#define | EPWM_ET_INTR_EVT_CNT_EQ_ZRO (PWMSS_EPWM_ETSEL_INTSEL_CTR_0) |
#define | EPWM_ET_INTR_EVT_CNT_EQ_PRD (PWMSS_EPWM_ETSEL_INTSEL_CTR_PERIOD) |
#define | EPWM_ET_INTR_EVT_CNT_EQ_CMPA_INC (PWMSS_EPWM_ETSEL_INTSEL_CTR_CMPA_INCR) |
#define | EPWM_ET_INTR_EVT_CNT_EQ_CMPA_DEC (PWMSS_EPWM_ETSEL_INTSEL_CTR_CMPA_DECR) |
#define | EPWM_ET_INTR_EVT_CNT_EQ_CMPB_INC (PWMSS_EPWM_ETSEL_INTSEL_CTR_CMPB_INCR) |
#define | EPWM_ET_INTR_EVT_CNT_EQ_CMPB_DEC (PWMSS_EPWM_ETSEL_INTSEL_CTR_CMPB_DECR) |
typedef uint32_t | Epwm_EtIntrEvt_t |
ePWM Interrupt (EPWMx_INT) Selection Options. More... | |
EPWM Interrupt (EPWMx_INT) Period Select | |
#define | EPWM_ET_INTR_PERIOD_DIS_INTR (PWMSS_EPWM_ETPS_INTPRD_DISABLE) |
#define | EPWM_ET_INTR_PERIOD_FIRST_EVT (PWMSS_EPWM_ETPS_INTPRD_GEN_FIRST_EVT) |
#define | EPWM_ET_INTR_PERIOD_SECOND_EVT (PWMSS_EPWM_ETPS_INTPRD_GEN_SECOND_EVT) |
#define | EPWM_ET_INTR_PERIOD_THIRD_EVT (PWMSS_EPWM_ETPS_INTPRD_GEN_THIRD_EVT) |
typedef uint32_t | Epwm_EtIntrPeriod_t |
ePWM Interrupt (EPWMx_INT) Period Select. These values determine how many selected events need to occur before an interrupt is generated. More... | |
Data Structures | |
struct | Epwm_TimebaseCfg_t |
Structure holding the TimeBase sub-module configuration parameters. More... | |
struct | Epwm_CounterCmpCfg_t |
Structure holding the Counter Comparator values. More... | |
struct | Epwm_AqActionCfg_t |
Structure holding the Action Qualifier actions to be taken on the PWM output at the specific events. More... | |
struct | Epwm_DeadbandCfg_t |
Structure holding the dead band generation sub-module configuration parameters. More... | |
struct | Epwm_ChopperCfg_t |
Structure holding the configuration parameters of Chopper sub-module. More... | |
struct | Epwm_TripzoneCfg_t |
Structure holding the trip-zone sub-module configuration parameters. More... | |
struct | Epwm_EtCfg_t |
Structure holding the Event Trigger Sub-Module configuration parameters. More... | |
Macros | |
#define | EPWM_ETFLG_INT_MASK (PWMSS_EPWM_ETFLG_INT_MASK) |
Mask used to check interrupt status. More... | |
Functions | |
void | Epwm_tbTimebaseClkCfg (uint32_t baseAddr, uint32_t tbClk, uint32_t moduleClk) |
This API configures the clock divider of the Time base module. More... | |
void | Epwm_tbPwmFreqCfg (uint32_t baseAddr, uint32_t tbClk, uint32_t pwmFreq, uint32_t counterDir, uint32_t enableShadowWrite) |
This API configures the PWM Time base counter Frequency/Period. More... | |
void | Epwm_tbSyncEnable (uint32_t baseAddr, uint32_t tbPhsValue, uint32_t counterDir) |
This API enables the synchronization of time base sub-module and also configures the phase count value to be loaded after sync event, counter direction after sync event. More... | |
void | Epwm_tbSyncDisable (uint32_t baseAddr) |
This API disables the synchronization. Even if sync-in event occurs the count value will not be reloaded. More... | |
void | Epwm_tbSetSyncOutMode (uint32_t baseAddr, uint32_t syncOutMode) |
This API selects the source of the synchronization output signal. It determines on which of the supported events sync-out has to be generated. More... | |
void | Epwm_tbTriggerSwSync (uint32_t baseAddr) |
This API generates software triggered sync pulse. More... | |
void | Epwm_tbWriteTbCount (uint32_t baseAddr, uint32_t tbCount) |
This API loads the Time base counter. The new value is taken immediately. More... | |
uint16_t | Epwm_tbReadTbCount (uint32_t baseAddr) |
This API gets the Time base counter current value. The count operation is not affected by the read. More... | |
uint16_t | Epwm_tbGetStatus (uint32_t baseAddr, uint32_t tbStatusMask) |
This API gets the Time Base status as indicated by the tbStatusMask parameter. More... | |
void | Epwm_tbStatusClear (uint32_t baseAddr, uint32_t tbStatusClrMask) |
This API clears the Time base status bits indicated by the tbStatusClrMask parameter. More... | |
void | Epwm_tbSetEmulationMode (uint32_t baseAddr, uint32_t mode) |
This API configures emulation mode. This setting determines the behaviour of Timebase counter during emulation (debugging). More... | |
uint32_t | Epwm_counterComparatorCfg (uint32_t baseAddr, uint32_t cmpType, uint32_t cmpVal, uint32_t enableShadowWrite, uint32_t shadowToActiveLoadTrigger, uint32_t overwriteShadow) |
This API configures the counter comparator and loads the comparator value. When Counter comparator value equals the counter value, then an event is generated both in the up direction and down direction. More... | |
void | Epwm_aqActionOnOutputCfg (uint32_t baseAddr, uint32_t pwmOutputCh, const Epwm_AqActionCfg_t *pCfg) |
This API configures the action to be taken on output by the Action qualifier module upon receiving the events. This will determine the output waveform. More... | |
void | Epwm_aqSwTriggerOneTimeAction (uint32_t baseAddr, uint32_t pwmOutputCh, uint32_t swTrigAction) |
This API triggers the SW forced single event on the PWM output. More... | |
void | Epwm_aqSwTriggerContAction (uint32_t baseAddr, uint32_t pwmOutputCh, uint32_t swTrigAction, uint32_t activeRegReloadMode) |
This API forces output value continuously on PWM output channel. The output can be forced to low or high. More... | |
void | Epwm_deadbandCfg (uint32_t baseAddr, const Epwm_DeadbandCfg_t *pCfg) |
This API performs the configuration of the dead band sub-module. This API configures the input source, output mode, polarity, rising and falling edge delays. More... | |
void | Epwm_deadbandBypass (uint32_t baseAddr) |
This API bypasses the Dead-band sub-module. More... | |
void | Epwm_chopperCfg (uint32_t baseAddr, const Epwm_ChopperCfg_t *pCfg) |
This API performs the configuration of the chopper sub-module. This API configures chopping clock duty cycle, chopping clock frequency and pulse width of first pulse of chopping clock. More... | |
void | Epwm_chopperEnable (uint32_t baseAddr, uint32_t enableChopper) |
This API controls the enabling or disabling of chopper sub-module. More... | |
void | Epwm_tzTriggerTripAction (uint32_t baseAddr, uint32_t tripAction, uint32_t pwmOutputCh) |
This API configures the o/p on PWM channel when a trip event is recognized. The output can be set to high or low or high impedance. More... | |
void | Epwm_tzTripEventEnable (uint32_t baseAddr, uint32_t tzEventType, uint32_t pinNum) |
This API enables the trip event. More... | |
void | Epwm_tzTripEventDisable (uint32_t baseAddr, uint32_t tzEventType, uint32_t pinNum) |
This API disable the trip event. The disabled trip events will be ignored. More... | |
void | Epwm_tzIntrEnable (uint32_t baseAddr, uint32_t tzEventType) |
This API enables the trip interrupt. When trip event occurs the sub-module can be configured to interrupt CPU. More... | |
void | Epwm_tzIntrDisable (uint32_t baseAddr, uint32_t tzEventType) |
This API disables the trip interrupt. More... | |
uint16_t | Epwm_tzEventStatus (uint32_t baseAddr, uint32_t eventMask) |
This API returns the selected trip zone event status. More... | |
void | Epwm_tzEventStatusClear (uint32_t baseAddr, uint32_t eventMask) |
This API clears the selected trip zone event status. More... | |
void | Epwm_tzTriggerSwEvent (uint32_t baseAddr, uint32_t tzEventType) |
This API enables to generate Software forced trip condition. More... | |
void | Epwm_etIntrCfg (uint32_t baseAddr, uint32_t intrEvtSrc, uint32_t intrPrd) |
This API configures the Event Trigger sub-module. This API configures the interrupt source and interrupt period. More... | |
void | Epwm_etIntrEnable (uint32_t baseAddr) |
This API enables the ePWM Event interrupt. More... | |
void | Epwm_etIntrDisable (uint32_t baseAddr) |
This API disables the ePWM Event interrupt. More... | |
uint16_t | Epwm_etIntrStatus (uint32_t baseAddr) |
This API returns the ePWM event interrupt status. More... | |
void | Epwm_etIntrClear (uint32_t baseAddr) |
This API clears the interrupt. This will clear the interrupt flag bit and enable further interrupts pulses to be generated. More... | |
void | Epwm_etIntrTrigger (uint32_t baseAddr) |
This API forces interrupt to be generated. This API is used for testing purpose. More... | |
uint16_t | Epwm_etGetEventCount (uint32_t baseAddr) |
This API returns the number of events occurred. More... | |