uint32_t PN_API_DEV_applyEquipmentConfiguration | ( | void | ) |
Apply equipment configuration.
Equipment of the device has to correspond some requirements to be able to provide services on PROFINET. Here the fulfilment of following requirements will be checked:
This function must be called to finalize equipment configuration after pulling / plugging of modules / submodules
PN_API_DEV_eOK | Equipment configuration is correct |
PN_API_DEV_eERROR_CONFIG_DAP_MISSING | DAP Module is missing. |
PN_API_DEV_eERROR_CONFIG_IM_DEVICE_REPRESENTATIVE_MISSING | No submodule was nominated as I&M device representative. |
PN_API_DEV_eERROR_CONFIG_IM_DEVICE_REPRESENTATIVE_INVALID | Submodule which is nominated as I&M device representative was configured wrongly . |