IO-Link Master  01.04.03
IOLM_SMI_SWPortConfigList Struct Reference

#include <IOLM_SMI_Types.h>

Data Fields

INT16U u16ArgBlockID
 Big endian.
 
INT8U u8PortMode
 
INT8U u8ValidationBackup
 
INT8U u8IQBehavior
 
INT8U u8PortCycleTime
 
INT16U u16VendorID
 Big endian.
 
INT32U u32DeviceID
 Big endian.
 
INT8U u8Slot
 slot number starting with 0
 
INT8U u8Track
 track number starting with 1
 
INT8U u8DeviceTxPower
 
INT8U u8MaxRetry
 
INT16U u16ImaTime
 Big endian. More...
 
INT8U u8SlotType
 0 = SSLOT / 1 = DSLOT.
 
INT8U u8LowPowerDevice
 0 = Normal Device / 1 = Low Power.
 
INT8U u8MaxPDSegLength
 
INT8U au8UniqueID [9]
 

Detailed Description

This structure is used to store wireless port configuration.

The ArgBlockID(IOLM_SMI_EArgBlockID) for this struct is IOLM_SMI_eArgBlockID_WPortConfigList = 0x8002.

Field Documentation

◆ u16ImaTime

INT16U IOLM_SMI_SWPortConfigList::u16ImaTime

Big endian.

<