Available CIP service codes.
Specifies which services are available on the CIP class or instance.
Enumerator |
---|
EI_API_CIP_eSC_GETATTRIBUTESALL | Returns the contents of the instance or class attributes defined in the object definition.
|
EI_API_CIP_eSC_RESET | Perform a reset.
|
EI_API_CIP_eSC_GETATTRSINGLE | Get_Attribute_Single is used to return the content of the specified attribute.
|
EI_API_CIP_eSC_SETATTRSINGLE | Set_Attribute_Single must be set if the attribute value should be modified.
|