EtherNet/IP™ Adapter  1.03.02
User Reference Manual

◆ EI_API_ADP_getACD()

uint32_t EI_API_ADP_getACD ( T *  pAdp_p,
bool *  pAcdEnabled_p 
)

Get the current address conflict detection setting (Instance Attribute ID: 10).

This function returns a boolean value indicating if Address Conflict Detection (ACD) is enabled or disabled.

Parameters
[in]pAdp_pPointer to the adapter.
[out]pAcdEnabled_pPointer to a boolean parameter that indicates if ACD is enabled.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
bool acdEnabled;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_getACD(pEI_API_ADP, &acdEnabled);
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:202
ETHIP_API uint32_t EI_API_ADP_getACD(T *pAdp_p, bool *pAcdEnabled_p)
Get the current address conflict detection setting (Instance Attribute ID: 10).
Definition: EI_API_ADP_main.c:2829
See also
EI_API_ADP_setACD EI_API_ADP_EError_t