EtherNet/IP™ Adapter  1.03.02
User Reference Manual

◆ EI_API_ADP_isDhcpEnabled()

uint32_t EI_API_ADP_isDhcpEnabled ( T *  pAdp_p,
bool *  pHwDhcpEnabled_p 
)

This function returns the hardware settings.

The function returns true if the hardware settings are enabled. Otherwise false.

Parameters
[in]pAdp_pPointer to the adapter.
[out]pHwDhcpEnabled_pPointer to a boolean that is set to true if DHCP is enabled by hardware settings and false if not.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
bool hwDhcpEnabled;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_isDhcpEnabled(pEI_API_ADP, &hwDhcpEnabled);
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:202
ETHIP_API uint32_t EI_API_ADP_isDhcpEnabled(T *pAdp_p, bool *pHwDhcpEnabled_p)
This function returns the hardware settings.
Definition: EI_API_ADP_main.c:3840
See also
EI_API_ADP_setHwSettings EI_API_ADP_EError_t